Arduino Forum Boost up communication's speed
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
  • State Not Answered
  • Replies 0 replies
  • Subscribers 390 subscribers
  • Views 152 views
  • Users 0 members are here
Related

Boost up communication's speed

strb
strb over 9 years ago

Hi, I have to sample a signal and then send it to pc, I've set the sample rate to 300Khz, the speed of the serial port to 500KByte/s and a single sample is an 8 bit number but my pc receives only 50Ksample/s(50Kbyte/s), can I reach a speed of 100/200Ksample or 50Ks is the maximum speed that I can use?How much time takes a Serial.print() instruction?

 

This is the arduino sketch:

 

byte mask=B01000000;//mask for start of conversion & state of conversion
boolean first=true;
char t=' ';

void setup()
{
  Serial.begin(4000000);//500kByte/s, super speed!
  ADMUX=B01100000;//I'm using input A0,result is left adjusted
  DIDR0=0x01;//shut off digital input for A0
  ADCSRA=B11000010;//I'm using 4 as division factor
  ADCSRB=0x00;//free running, default setting
}

void loop()
{
  if(first)//do it only the first time
  {
    startofconversion();
    first=false;
  }
  
    t=waitandget();
    Serial.print(t);//send data
    startofconversion();//start a new conversion
}

void startofconversion()
{
  ADCSRA=ADCSRA|mask;//let's start a conversion!
}

byte waitandget()
{
  while((ADCSRA&mask)==mask)//wait
  {
  }

  return ADCH;
}