Arduino Forum Tri-State Buffer
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
  • State Suggested Answer
  • Replies 6 replies
  • Answers 2 answers
  • Subscribers 404 subscribers
  • Views 947 views
  • Users 0 members are here
  • transistor
  • buffer
Related

Tri-State Buffer

timswift
timswift over 9 years ago

Could I use a transistor for a tri-state buffer?

 

Tim

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago in reply to timswift +1 suggested
    Then for sure you need a true tri-state buffer and possibly one with a built in latch, perhaps these may help http://www.ti.com/lit/ds/snos333a/snos333a.pdf
Parents
  • D_Hersey
    0 D_Hersey over 9 years ago

    Peter O, if I am interpreting him rightly, is referring to a totem-pole output with a passive pull-up.    Often called wire-or or wire-and.  This can act as another layer of logic, especially useful if the ultimate number of inputs is unknown.  Open collector devices are designed for this, but you can make a complementary/symmetry output like like OC with a diode.  You can do tricks like this with TS, sometimes you have to use diodes to protect from simultaneous events.  If you talk more about your intention, we can find the more appropriate method.

     

    If you have OC but want pseudo-complementary/symmetry, you can use a current source for a top-load.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • D_Hersey
    0 D_Hersey over 9 years ago

    Peter O, if I am interpreting him rightly, is referring to a totem-pole output with a passive pull-up.    Often called wire-or or wire-and.  This can act as another layer of logic, especially useful if the ultimate number of inputs is unknown.  Open collector devices are designed for this, but you can make a complementary/symmetry output like like OC with a diode.  You can do tricks like this with TS, sometimes you have to use diodes to protect from simultaneous events.  If you talk more about your intention, we can find the more appropriate method.

     

    If you have OC but want pseudo-complementary/symmetry, you can use a current source for a top-load.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • timswift
    0 timswift over 9 years ago in reply to D_Hersey

    Thanks for the fast reply's.

     

    A latch is not needed .  I am only connecting the value on the sram to the bus so the A register can read it. 

     

     

    Tim