Arduino Forum Using PORT() for data
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
  • State Verified Answer
  • Replies 9 replies
  • Answers 4 answers
  • Subscribers 391 subscribers
  • Views 664 views
  • Users 0 members are here
  • strings
  • 7-segment-display
  • port manuplation
Related

Using PORT() for data

billpenner
billpenner over 9 years ago

This is probably a very easy question for someone out there but It has me stumped. I have a three digit number like 123 or 286 etc. I am sending it from a Mega to NRF24l01+. This is working fine.

I am receiving the number fine with another NRF24l01+ and a Nano. now the problem. I have a 3 digit, 7 segment display. It is also working fine when using this code for a test..

 

[code]

/*Select a seven segment digit () in sequence.

* load a value into display for testing

*/

int i ;

byte j = B0000 ;              //the digit value (0 to 9)

 

void setup()

{

   DDRC = DDRC | B00111111;    // set PORT C (digital 5~0) to outputs

  pinMode(6, OUTPUT);               // digit select pins (Latch signal)

  pinMode(7, OUTPUT);

  pinMode(8, OUTPUT);

Serial.begin(9600);

}

 

void loop() {

for (i = 6; i <9 ; i++)       //digit select latch

  {

  digitalWrite(i, HIGH);      // open latch

    delay(100);

    for (j = 0; j <10 ;  j++) // test values for the display

     {

       PORTC = j;             // write HEX value to digit

      // Serial.print( PORTD ) ;    // just for testing

      // Serial.print( PORTC ) ;     // just for testing

       delay(100); //

     }

     delay(500);  // wait a bit to read digit

     digitalWrite(i, LOW);      // close latch

     delay(1000);

       Serial.println( byte(i)) ; //only for testing

   }

   if(i == 9, i=6);  //reset digit counter and do it again

}

[/code]

when I run the above code each digit counts up the latches then the next digit counts up. At he end.all is reset and repeats.

My problem is I can't isolate each of the received digits to individually load them into the display. Is there a way to separate the received number into digits so I can load the port? I hope this makes sense.

I can supply the schematic, video, etc.  if it would help.

 

Bill

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 9 years ago

    I think you need this Adafruit customer service forums • View topic - How to convert a string to a number . It can take 1 cgar at a time and convert to a number.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • billpenner
    0 billpenner over 9 years ago in reply to clem57

    I think both these do about the same thing, but I am separating the digits from the number not building a number from the digits.

    Thanks again everybody.

    ps. How do I do a "Helpful"? I see the "Correct answer" but I would like to also do Helpful.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 9 years ago in reply to billpenner

    Below each post is  :

     

    Like Show 0 Likes(0) • Helpful Yes | No • Comment • ReportActions

     

    Click on Yes if helpful.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 9 years ago in reply to billpenner

    Below each post is  :

     

    Like Show 0 Likes(0) • Helpful Yes | No • Comment • ReportActions

     

    Click on Yes if helpful.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • billpenner
    0 billpenner over 9 years ago in reply to clem57

    OK I got it. I tried to mark them without signing in.

    They show up now.

    Thanks,

    Bill