Arduino
  • Products
  • More
Arduino
Arduino Forum How can I attach four separate buttons to a single interrupt?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 12 replies
  • Answers 4 answers
  • Subscribers 410 subscribers
  • Views 2136 views
  • Users 0 members are here
  • interrupt
  • multiple_buttons
  • low power
  • atmega328
  • arduino
Related

How can I attach four separate buttons to a single interrupt?

bwarren97
bwarren97 over 10 years ago

I'm working on a project that I've been pondering for almost a year, and I have been prototyping it with my Arduino Mega 2560 (my Arduino mini died, so the 2560 is all I have at the moment) for the past two weeks, but I've hit a snag.

 

Here's a little breakdown: I have four buttons I want on the final product. I have each button defined as pins in my script.

I want the ATMEGA to power down when I press one of these buttons, or after a set amount of time being idle. Then, I want to be able to press any one of my buttons to power it back on again.

 

Since my final product is going to use an ATMEGA328 instead of a 2560, that means I can really only use one of the two interrupts (right?) to wake the chip. It also simplifies my software quite a bit if I can use one pin to power the buttons and detect that a button was pressed, and the other pins to detect which button was pressed. So I've set up my buttons so that the wake pin is pulled high, and the button pins are pulled low, and when I press a button, theoretically, the wake pin goes low and the button pin goes high. Doesn't happen. The wake pin does go low, but the button pin doesn't go high, and I can't figure out why. Even if I remove the pull-down resistor, it doesn't work.

 

Does anyone have any ideas?

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 10 years ago +3 suggested
    There are several ways to solve this - if I understand it correctly. One way is to use double pole switches, where one pole on each switch drives a corresponding button pin, and the other poles are all…
  • bwarren97
    bwarren97 over 10 years ago in reply to Robert Peter Oakes +3
    Yes. I just now made the changes to my script and it works exactly as it should. I thank everyone for the suggestions!
  • bwarren97
    bwarren97 over 10 years ago in reply to dougw +2
    I like the double-pole switch idea, but I like the diode idea better. Is this what you were talking about? I labeled the lines that would connect to the microcontroller
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago

    First of, if you are driving the bottom of a button low and the top is to another pin that is an input with a pull up, then I would simply look for that pin going low and use it to trigger the interrupt.

     

    Now if you want the MPU to be asleep then output all bottom pins of the switches to low so that any one of them being pressed will pull the input pin low, then the ISR will scan the pins quickly by having only one button low at a time to determine the one that is pressed

     

    You can't balance a pull up on one side of a switch and a pull down on the other and hope they're going to swap states when the button is pressed, at best the voltage will go to a mid and undetermined voltage which is not good. you need a solid pull to zero volts by using the pin as an output

     

    I hope that helps you out

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gihu
    0 gihu over 10 years ago in reply to Robert Peter Oakes

    I like the dougw proposal. Making an and gate with diodes with an internal pull-up for the interrupt input, and each katode to each input.

    Just be carefull of a very important thing, Vf of the diode must be less than 0.3Vcc, it should not be a problem for 5V or even 3.3V, but I can be for lower voltages.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 10 years ago in reply to gihu

    Isn't that an or gate?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Jan Cumps
    0 Jan Cumps over 10 years ago in reply to gihu

    Isn't that an or gate?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • gihu
    0 gihu over 10 years ago in reply to Jan Cumps

    Hi Jan

     

    If you use internal pull-up resistors, you make the interrupt when input is low, the normal status for the inputs is high, and as soon as you have a low at any input, you have a low in the interrupt:

    1  1 -> 1

    1  0 -> 0

    0  1 -> 0

    0  0 -> 0

    That's an and gate.

    You can use diodes in a or-gate way, connecting all the katodes to the interrupt pin (and each anode to each input pin), but then the interurpt should be active by high, instead of low, and you have to use external pull down resistors, instead of internal pull-up, of course, the inputs should work also with pull down resistors in this case, where as soon as you get a high at any input, you will have a high at the interrupt.

    0 0 -> 0

    0 1 -> 1

    1 0 -> 1

    1 1 -> 1

    That's an or gate

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gihu
    0 gihu over 10 years ago in reply to Jan Cumps

    I know I am not a very good at explaning.

    Maybe an image it is better:

    Diode Logic Gates

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 10 years ago in reply to gihu

    You are correct.