Arduino Forum Brushless Motor Controller
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
  • State Not Answered
  • Replies 3 replies
  • Subscribers 403 subscribers
  • Views 418 views
  • Users 0 members are here
  • bldc motor control
Related

Brushless Motor Controller

Former Member
Former Member over 9 years ago

Hi, hopefully someone here would be kind enough to help me out or point me in the right direction or to the right place to ask this.

 

I'm working on a project requiring a BLDC motor controller for a 48V system, up to 10 amps or so continuous. Here's the catch: I can't use a premade controller or controller IC. So, I made the board attached. Essentially what happens is PWM signal (from an Arduino that's reading the motor Hall sensors. 400 Hz, not sure if it'd be beneficial to increase frequency?) comes in the jumper pins, goes to gate drivers, which then drives MOSFETs that should connect the different phases of the motor high/low as needed. It hasn't been working, and I'm not quite sure why, even after a lot of troubleshooting. Perhaps I'm trying t draw too much current and pushing the FETs outside the safe operating area? I'm a mechanical engineering student, so it's entirely possible I completely screwed something up.

 

If anyone has done something similar or has any ideas, I would greatly appreciate it!

 

P.S. The top portion of the board is just an experiment trying to convert to 12V on the board, it's not on the physical copy of the board I have.

Attachments:
image
image
  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 9 years ago +1
    Hi Trent, What is the supply voltage (VCC)? It is 12V or so, right? (i.e. not the Arduino 5V supply). Also, you might want to (carefully!!) monitor the voltage on the VB pin with no motor connected, at…
  • clem57
    clem57 over 9 years ago in reply to shabaz +1
    The comment from shabaz should be taken to heart because your have both high direct voltage with a lot of current(power). I am guessing you are a student. Why can try with a small scaled version before…
  • peterjcs23
    peterjcs23 over 9 years ago +1
    ...you don't appear to have any shoot-through prevention in your circuit hardware and it did not sound like you have it in software, which would be tricky to get the timing right from a general purpose…
Parents
  • shabaz
    0 shabaz over 9 years ago

    Hi Trent,

     

    What is the supply voltage (VCC)? It is 12V or so, right? (i.e. not the Arduino 5V supply).

    Also, you might want to (carefully!!) monitor the voltage on the VB pin with no motor connected, at different speeds, i.e.

    as you would if you were ramping up the motor from stop to full speed.

    Probably very worthwhile using a voltage divider there (with high resistor values to keep discharge impact low) before you connect to your scope input!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 9 years ago

    Hi Trent,

     

    What is the supply voltage (VCC)? It is 12V or so, right? (i.e. not the Arduino 5V supply).

    Also, you might want to (carefully!!) monitor the voltage on the VB pin with no motor connected, at different speeds, i.e.

    as you would if you were ramping up the motor from stop to full speed.

    Probably very worthwhile using a voltage divider there (with high resistor values to keep discharge impact low) before you connect to your scope input!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • clem57
    0 clem57 over 9 years ago in reply to shabaz

    The comment from shabaz should be taken to heart because your have both high direct voltage with a lot of current(power). I am guessing you are a student. Why can try with a small scaled version before going large? The learning you will get is more valuable and making mistakes less of a burden. In true learning mistakes help more than answers.

    Clem