Arduino
  • Products
  • More
Arduino
Arduino Forum arduino to arduino wireless communication
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 12 replies
  • Answers 2 answers
  • Subscribers 418 subscribers
  • Views 2776 views
  • Users 0 members are here
  • arduino rf
  • arduino-robot
  • arduino uno
  • help
  • arduino-compatible
  • arduino shield
  • arduin_network
  • arduino sensor
  • arduino
  • question
Related

arduino to arduino wireless communication

e14 Contributor
e14 Contributor over 10 years ago

Hello,

 

i am working on a project that requires wireless control of 5 servos,,first analog values are taken form sensors and transmitted.

i am new to working with arduino, and do not have much knowledge about wireless arduino comm.

how can i achieve this?

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 10 years ago +1 suggested
    Hi Anshuman, Some more information is needed on your scenario unfortunately, in order to give a higher quality answer. Wireless could mean across the world. Also the actual scenario and what you intend…
  • strb
    strb over 10 years ago +1
    You can use anly one tramitter and 5 receiver that all receive the same signal in a single channel and at the end of each receiver an arduino (as shabaz say) or you can also use an attiny that is less…
  • gadget.iom
    gadget.iom over 10 years ago in reply to e14 Contributor +1
    Some code/schematics/photos of your wired version would help us to understand what you are trying to achieve.
Parents
  • strb
    0 strb over 10 years ago

    You can use anly one tramitter and 5 receiver that all receive the same signal in a single channel and at the end of each receiver an arduino (as shabaz say) or you  can also use an attiny that is less expensive than an atmega 328. To transmitt data you can divide your packet into two pieces: an header with a code that specify what servo you are controlling and the data piece thet you can use to trasmitt a number that means the position that the servo have to reach, the microcontroller at the receiver only translate the data if the header that receive is correct so you can control all servos using a single channel.

    Hope that this will help.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to strb

    With the setup strbhas suggested which is great, add a piece to the message sent back to the Arduino to say who is talking back.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 10 years ago in reply to strb

    With the setup strbhas suggested which is great, add a piece to the message sent back to the Arduino to say who is talking back.

    Clem