Arduino Forum Multiple slave devices to one arduino master...
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
  • State Not Answered
  • Replies 3 replies
  • Subscribers 392 subscribers
  • Views 707 views
  • Users 0 members are here
  • arduino master slave prlm
Related

Multiple slave devices to one arduino master...

Former Member
Former Member over 9 years ago

hey... i am trying to couple few sensors in arduino Uno.. my main aim is to use the lcd 1602 display a message as in "insert ur card".. thn rfid mfrc522 sacns the card.. n displays the message on lcd... also i need to activate the gsm sim900a modem and gps to take the location n speed and keep storing them...
i got success with getting the code individually but when i combine the code...

 

firstly the LCD and RFID when combined togethr only the lcd works and control is not passed to RFID and the same in case of GPS...

 

I have done quite research on this topis as well.. n i hav reached to one thing tht is SPI or I2c.. bt i dnt want to increase anothr hardware by using I2C...
so can i do something with SPI???

 

but even there is dbt with that cz.. SPI requires the ss pin , address of all the slave devices..
but i dont know the slave select pin for lcd , gsm and gps cz there is no CS or SS pin on their hardware... so which pin should i initialise as SS for them??
Can someone help asap... its little urgent as its my final yr projct..
i am attaching the code below fr reference...
Thanks in advance...

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 9 years ago

    Pictures would help with schematics.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 9 years ago

    Pictures would help with schematics.