Arduino
  • Products
  • More
Arduino
Arduino Forum Is it possible to reset the Arduino with a software command?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 22 replies
  • Answers 5 answers
  • Subscribers 419 subscribers
  • Views 5401 views
  • Users 0 members are here
Related

Is it possible to reset the Arduino with a software command?

billpenner
billpenner over 10 years ago

I am now resetting using  "asm volatile ("  jmp 0"); and it works but I would like to leave the variables as is. I want to leave the LCD backlight off. I can supply the code if necessary.

Thanks, Bill

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +2 suggested
    essentially it would be as if you hit the reset button. Remember the Arduino code is at a very high level, abstracting much of the hardware and even code from the developer, the typical developer using…
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to shabaz +2
    Oh so true But a fun road to travel, as with many things, the trip can be more fun that the destination
  • shabaz
    shabaz over 10 years ago +1 suggested
    Hi Bill, That may be tricky, depending on the scope some variables are set to zero automatically, and others will have different content (i.e. non-zero). However, one option is to write your data to EEPROM…
Parents
  • shabaz
    0 shabaz over 10 years ago

    Hi Bill,

     

    That may be tricky, depending on the scope some variables are set to zero automatically, and others will have different content (i.e. non-zero).

    However, one option is to write your data to EEPROM, which of course is persistent even after power loss.

    Is there a reason you wish to reset? Ordinarily you'd never do that (unless a software failure was detected, e.g. using a watchdog timer)

    or some rare scenario like a software upgrade. (normal practice is to never allow have the microcontroller to reset or exit).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • billpenner
    0 billpenner over 10 years ago in reply to shabaz

    The display sets idle for a long time  (hours) then when a keypress happens, the backlight comes on until the current function completes.

    Thanks for the thought.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • billpenner
    0 billpenner over 10 years ago in reply to shabaz

    The display sets idle for a long time  (hours) then when a keypress happens, the backlight comes on until the current function completes.

    Thanks for the thought.