Arduino
  • Products
  • More
Arduino
Arduino Forum Is it possible to reset the Arduino with a software command?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 22 replies
  • Answers 5 answers
  • Subscribers 419 subscribers
  • Views 5407 views
  • Users 0 members are here
Related

Is it possible to reset the Arduino with a software command?

billpenner
billpenner over 10 years ago

I am now resetting using  "asm volatile ("  jmp 0"); and it works but I would like to leave the variables as is. I want to leave the LCD backlight off. I can supply the code if necessary.

Thanks, Bill

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +2 suggested
    essentially it would be as if you hit the reset button. Remember the Arduino code is at a very high level, abstracting much of the hardware and even code from the developer, the typical developer using…
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to shabaz +2
    Oh so true But a fun road to travel, as with many things, the trip can be more fun that the destination
  • shabaz
    shabaz over 10 years ago +1 suggested
    Hi Bill, That may be tricky, depending on the scope some variables are set to zero automatically, and others will have different content (i.e. non-zero). However, one option is to write your data to EEPROM…
Parents
  • tonyboubady
    0 tonyboubady over 10 years ago

    Maybe I/O pin controlling the backlight of LCD using transistor? On click of the button(which the I/O pin connected to base of the transistor) the transistor switch on the LCD backlight with timer and goes off after a minute or so...and waiting for user keypress... exactly like how mobile/tablet screen works...I am not sure what type of LCD you use but I can use this method with 16x2 LCD.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • tonyboubady
    0 tonyboubady over 10 years ago

    Maybe I/O pin controlling the backlight of LCD using transistor? On click of the button(which the I/O pin connected to base of the transistor) the transistor switch on the LCD backlight with timer and goes off after a minute or so...and waiting for user keypress... exactly like how mobile/tablet screen works...I am not sure what type of LCD you use but I can use this method with 16x2 LCD.