Arduino
  • Products
  • More
Arduino
Arduino Forum Is it possible to reset the Arduino with a software command?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 22 replies
  • Answers 5 answers
  • Subscribers 419 subscribers
  • Views 5398 views
  • Users 0 members are here
Related

Is it possible to reset the Arduino with a software command?

billpenner
billpenner over 10 years ago

I am now resetting using  "asm volatile ("  jmp 0"); and it works but I would like to leave the variables as is. I want to leave the LCD backlight off. I can supply the code if necessary.

Thanks, Bill

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +2 suggested
    essentially it would be as if you hit the reset button. Remember the Arduino code is at a very high level, abstracting much of the hardware and even code from the developer, the typical developer using…
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to shabaz +2
    Oh so true But a fun road to travel, as with many things, the trip can be more fun that the destination
  • shabaz
    shabaz over 10 years ago +1 suggested
    Hi Bill, That may be tricky, depending on the scope some variables are set to zero automatically, and others will have different content (i.e. non-zero). However, one option is to write your data to EEPROM…
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago

    essentially it would be as if you hit the reset button. Remember the Arduino code is at a very high level, abstracting much of the hardware and even code from the developer, the typical developer using "Wiring" to code the arduino is not even close to the machine. The watchDog Timer will trigger a reset by entering into a defined address and executing the code found there, this is all explained in the linked article I provided. It is not quite the same as powering off then on, but it is as close to hitting the reset button as you can get.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • billpenner
    0 billpenner over 10 years ago in reply to Robert Peter Oakes

    It seems that watchdog timer, Interrupt, reset button, and asm volatile ("  jmp 0") , will do the same thing except that watchdog timer and Interrupt sends code execution to a specified place. Also the interrupt requires a physical connection. Maybe I should add a MC switch on the reset pin? The case is already built but that is also a possibility. Please  also see my response to shabaz.

    Bill

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • billpenner
    0 billpenner over 10 years ago in reply to Robert Peter Oakes

    It seems that watchdog timer, Interrupt, reset button, and asm volatile ("  jmp 0") , will do the same thing except that watchdog timer and Interrupt sends code execution to a specified place. Also the interrupt requires a physical connection. Maybe I should add a MC switch on the reset pin? The case is already built but that is also a possibility. Please  also see my response to shabaz.

    Bill