Arduino
  • Products
  • More
Arduino
Arduino Forum ARDUINO UNO + SIM808 GPS/GSM/GPRS MODULE SYNCHRONISATION PROBLEM
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 402 subscribers
  • Views 551 views
  • Users 0 members are here
  • sim808
Related

ARDUINO UNO + SIM808 GPS/GSM/GPRS MODULE SYNCHRONISATION PROBLEM

Former Member
Former Member over 9 years ago

HELLO everyone,

 

i started a project quite recently were i intend to combine the arduino uno and the sim808 module which has gps/gsm/gprs all together in one.

 

using just the gps functionality works fine, just the gsm both recieving and sending messages also works good. but combining them for what i intend makes the entire system falls apart.

 

i intend to be able to have some coordinates registered lets say position A position B and position c, and the system i intend to design is put on a moving, lets say car, now anyone on either of the positions will send a message with the alphabet denoting the position to a number lets say "A TO +23*******98 , AND WOULD get a reply of the cars current time from that position.

 

with all parts combined the program would sometimes not even indicate recieving any message or evn if it did the gps part wont even work.

 

is there something i am doing wrong or is it not just feasible with what the components i am using

pls help as i very confused right now. thanks in advance

 

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 9 years ago

    It is simple to do one timing function correctly. Or to do another okay. But combine them together is tricky even for the seasoned pro. Why? Because while you are handling one event, the other needs to work or check something. The way to handle them is called asynchronous programming and is possible if and only if the library routines allow it. See http://stackoverflow.com/questions/748175/asynchronous-vs-synchronous-execution-what-does-it-really-mean

    or http://cs.brown.edu/courses/cs168/f12/handouts/async.pdf.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 9 years ago in reply to clem57

    WOULD GET RIGHT ON THAT TRACK. THANKS

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 9 years ago in reply to clem57

    WOULD GET RIGHT ON THAT TRACK. THANKS
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
An Avnet Company © 2025 Premier Farnell Limited. All Rights Reserved.