Arduino
  • Products
  • More
Arduino
Arduino Forum Reading PWM Signals With The Arduino
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 417 subscribers
  • Views 5648 views
  • Users 0 members are here
  • pwm
  • reading
  • arduino
Related

Reading PWM Signals With The Arduino

timswift
timswift over 10 years ago

How would i set about reading PWM signals with the Arduino

and converting them into a more easily used format (like a number from 0 to 180). 

 

Thanks

 

  Tim

  • Sign in to reply
  • Cancel

Top Replies

  • clem57
    clem57 over 10 years ago +1 suggested
    https://www.arduino.cc/en/Tutorial/PWM is how and quite easy to create a PWM. But you asked how to read. This is much harder since we have to talk about rising and falling edges. A good look is http:/…
Parents
  • clem57
    0 clem57 over 10 years ago

    https://www.arduino.cc/en/Tutorial/PWM is how and quite easy to create a PWM. But you asked how to read. This is much harder since we have to talk about rising and falling edges. A good look is http://www.benripley.com/diy/arduino/three-ways-to-read-a-pwm-signal-with-arduino/ Once you say use method one, you need to convert that into a 0-180 scale by saying 100% equal 180 and 0% equal 0 over a fixed time domain. Another more interesting way using an Arduino is Arduino - SecretsOfArduinoPWM . But this is hardware specific.

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 10 years ago

    https://www.arduino.cc/en/Tutorial/PWM is how and quite easy to create a PWM. But you asked how to read. This is much harder since we have to talk about rising and falling edges. A good look is http://www.benripley.com/diy/arduino/three-ways-to-read-a-pwm-signal-with-arduino/ Once you say use method one, you need to convert that into a 0-180 scale by saying 100% equal 180 and 0% equal 0 over a fixed time domain. Another more interesting way using an Arduino is Arduino - SecretsOfArduinoPWM . But this is hardware specific.

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • timswift
    0 timswift over 10 years ago in reply to clem57

    It works!

    I used method one and it is a vary small amount of code.

     

     

    Tim