Arduino Forum Why does my " +IPD,<len>: " AT command executes only once even if placed in void loop() ?
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
  • State Not Answered
  • Replies 0 replies
  • Subscribers 400 subscribers
  • Views 369 views
  • Users 0 members are here
  • +ipd
  • esp8266
  • iot;
  • serial monitor
  • uno
  • at commands
  • arduino
Related

Why does my " +IPD,<len>: " AT command executes only once even if placed in void loop() ?

Former Member
Former Member over 9 years ago

I want to run all AT commands through Arduino Code over the Serial Monitor,and want to fetch data using a Thingspeak Key.

My other AT commands execute well periodically as needed in void loop(), but whenever I place the " +IPD,<len>: " AT command into void loop(), the loop() function runs only once and stops.

 

 

Need help in fixing this problem. Reply as soon as you can.

My UNO Code is as follows  :

 

#include <LiquidCrystal.h>

#include <SoftwareSerial.h>

 

 

// We'll use a software serial interface to connect to ESP8266

SoftwareSerial ESP8266 (8,9); //rx=8,connected to 9 of arduino. tx=9, connected to 8 of arduino

 

LiquidCrystal lcd(12,11,5,4,3,2);

String inData;

 

 

void setup()

{

  Serial.begin(9600);

  ESP8266.begin(9600);

  lcd.begin(16,2);                                 

  delay(1000); // Let the module self-initialize

 

 

  ESP8266.println("AT");

 

  while(ESP8266.available())

  Serial.write(ESP8266.read());

  lcd.print("OK");

  lcd.clear();

  delay(1500);

  lcd.setCursor(0,0);

 

  ESP8266.println("AT+CWJAP?");

  while(ESP8266.available()) 

  delay(2000);

  Serial.write(ESP8266.read());

 

 

 

}

 

 

void loop()

{

  delay(2500);

  ESP8266.println("AT+CIPSTART=\"TCP\",\"api.thingspeak.com\",80\r\n");

  while(ESP8266.available())

  delay(1500);

  Serial.write(ESP8266.read());

  delay(1000);

  ESP8266.println("AT+CIPSEND=50\r\n");

  while(ESP8266.available())

  Serial.write(ESP8266.read());

  delay(1500);

 

 

  boolean b = Serial.find(">");

 

  if(b)

  {

    String hostt = "GET /apps/thinghttp/send_request?api_key=689WYA85WW1VJSBA";

    hostt += "\r\n";

    hostt += "Host:api.thingspeak.com";

    hostt += "\r\n\r\n\r\n\r\n\r\n\r\n";

    ESP8266.println(hostt);

    delay(3000);

  }

 

 

  ESP8266.print("+IPD,12:");

  delay(1500);

  String inData = ESP8266.readString();

  Serial.write(ESP8266.read());

   

  /*.....................Fetching Data Needed..................*/

 

 

 

 

  int i = ':';   

  while (inData.charAt(i) != ':') // Character before required data starts.

     i++;

     inData = inData.substring(i);

 

     int j = 0;

  while (inData.charAt(j) != 'C') // Character after required data ends.

     j++;

     inData = inData.substring(0, j);

  Serial.print(inData);

    

  delay(3000);

  delay(5000);

 

  ESP8266.println("AT+CIPCLOSE\r\n");

  while(ESP8266.available())

  Serial.write(ESP8266.read());

  delay(4000); 

 

 

}