Arduino Forum how make time depend
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
  • State Suggested Answer
  • Replies 5 replies
  • Answers 1 answer
  • Subscribers 403 subscribers
  • Views 573 views
  • Users 0 members are here
Related

how make time depend

Former Member
Former Member over 9 years ago

Hi there, my frist post, on e14 community (just to you know, im a nurse in a nursing home, have some experience in arduino, (copy/past coding, and i have an quadcopter based in the Ardupilot)

Now my problem, i have an pacient with Alzheimer disease, that fall asleep in the toilet, some times more than an hour, i want to use an HC-SR04 range finder to make a simple task: (a detail the toilet is used by other that use regularly the toilet)

Scanning distance to target (person sit on toilet)

IF is less to 50cm AND for more than 10min

Activate LED

Activate a Servo ( to pull the emergency bell)

Loop

Now im trying to learn the code, and i understand the code for range findings, and millis (to time), but i didint get the way to make the statemant IF => 50 && 6000sec

Cant see a way to create the code

image

I hope you help me

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 9 years ago +1 suggested
    Hi Jorge, Sorry I can't answer your specific question but I will throw out an idea anyway. The bathroom in the nursing home where my mother is a resident has a sensor for the light switch. When someone…
  • jw0752
    jw0752 over 9 years ago +1
    Are you in a location where they will let you interface and modify nursing home electronic systems? This has been a problem for me as I have attempted to help my mother in her situation with adaptive technology…
Parents
  • phoenixcomm
    0 phoenixcomm over 9 years ago

    I think that everybody missed the boat!! KISS!! Keep It Simple Stupid.

    instead of all this sensor stuff is:

    1. IR diode tx

    2. IR diode receiver.

    3. double sided tape or command strip for mounting, the gizmo(s).

    A) position diodes across from one another at the level of the Tush, ie. backside.  This is all you need really no programming.

    power up the IRtx which turns on the IRrx.

    B) when the Tush brakes the beam, Now start your timer.

    C) No Mess, No Fuss

    OR if you really need an occupancy sensor just a photodiode should work fine. (you want to shield it away from direct light, and you can calibrate it if you use an analog input.)

     

    Cris H.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • phoenixcomm
    0 phoenixcomm over 9 years ago

    I think that everybody missed the boat!! KISS!! Keep It Simple Stupid.

    instead of all this sensor stuff is:

    1. IR diode tx

    2. IR diode receiver.

    3. double sided tape or command strip for mounting, the gizmo(s).

    A) position diodes across from one another at the level of the Tush, ie. backside.  This is all you need really no programming.

    power up the IRtx which turns on the IRrx.

    B) when the Tush brakes the beam, Now start your timer.

    C) No Mess, No Fuss

    OR if you really need an occupancy sensor just a photodiode should work fine. (you want to shield it away from direct light, and you can calibrate it if you use an analog input.)

     

    Cris H.