Arduino Forum Making a Compartmental Arduino Qwerty Keyboard
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
  • State Verified Answer
  • Replies 16 replies
  • Answers 5 answers
  • Subscribers 394 subscribers
  • Views 1623 views
  • Users 0 members are here
  • keyboard
  • diy
  • arduino
  • question
Related

Making a Compartmental Arduino Qwerty Keyboard

Former Member
Former Member over 9 years ago

While I can find ways to add a single keyboard matrix to an arduino Leonardo to make it a keyboard (Qwerty Keyboard) for most computers, I'm looking to make a compartmental keyboard with an arduino.  That way I can start with making a gaming keypad and switch it over to an ergonomic keyboard and maybe latter be able to add arcade type attachments, additional macros, or maybe a custom mouse.  I know this is a bit of a advanced project for a beginner, but I just plan to start with a gaming pad.  My question is, which arduino would be best to start with?  I have thus far looked at the Leonardo because of its built in HID and libraries, but I don't know if there is enough inputs for the number of eventual interfaces I might use.  I'm also looking at the Mega and Due, but I'm not sure the Mega will be workable and the Due offers the additional challenge of guarding against over-volting the board and many types of interface boards use higher voltages.  Any Input and suggestions will be greatly appreciated.

 

Thank you in advance.

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 9 years ago in reply to Jan Cumps +5 suggested
    I watched a very interesting documentary on Linotype and how it revolutionised both printing and literacy in general due to the reduced cost of print. Their keyboard was based on the most used lower case…
  • Former Member
    Former Member over 9 years ago in reply to Jan Cumps +3
    Because if you just use keyboard most of the time it's assumed you are making a midi keyboard. I use qwerty as a description for a alpha Numeric keyboard. Additionally I do plan to make the keyboard so…
  • Former Member
    Former Member over 9 years ago in reply to clem57 +2
    I thought about using the PI, but thought that the nature of raspberry design might cause too much latency. I'll research using a PI and PI Zero. Thank you.
Parents
  • phoenixcomm
    0 phoenixcomm over 5 years ago

    Hi, I personaly don't like shift regs to get data out of the cpu. If you are using Regualar Keyboard there are aproxamently 6 rows (5 with out functions) and  14 cols with out right, left, up, down, etc, and then the right side keypad. First scanning is a waste of CPU time. So, here is what I would do.  to get six rows from the cpu drive via Priopity Encoder 7 bit (there expandable). so now where down to three bits. (0-6) then for you colloumns you can use the Priority Encoders (3 with them hooked to gethere will give you 24 cols(max) with out external gates. (thats 5bits).

    Now for some fun.

    cpu i/o 0-2-4 drive

    get a i2c port expander 0-2-4-8-16  So far so good?

    on the port expander there is an interupt output (low active)

    So when the expander sees the interupt

    it scans the the port expander (pulled down) that tells you what column and the row is self evedance.

     

    Fins Have a Beer!!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • phoenixcomm
    0 phoenixcomm over 5 years ago

    Hi, I personaly don't like shift regs to get data out of the cpu. If you are using Regualar Keyboard there are aproxamently 6 rows (5 with out functions) and  14 cols with out right, left, up, down, etc, and then the right side keypad. First scanning is a waste of CPU time. So, here is what I would do.  to get six rows from the cpu drive via Priopity Encoder 7 bit (there expandable). so now where down to three bits. (0-6) then for you colloumns you can use the Priority Encoders (3 with them hooked to gethere will give you 24 cols(max) with out external gates. (thats 5bits).

    Now for some fun.

    cpu i/o 0-2-4 drive

    get a i2c port expander 0-2-4-8-16  So far so good?

    on the port expander there is an interupt output (low active)

    So when the expander sees the interupt

    it scans the the port expander (pulled down) that tells you what column and the row is self evedance.

     

    Fins Have a Beer!!