Arduino Forum Use a uni-polar stepper in place of a bi-polar stepper
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
  • State Verified Answer
  • Replies 9 replies
  • Subscribers 394 subscribers
  • Views 683 views
  • Users 0 members are here
  • stepper motor
  • stepper
Related

Use a uni-polar stepper in place of a bi-polar stepper

gub11
gub11 over 9 years ago

I have an instructables (Frameless Laser Harp ) that I attempted to build about 6 months ago, but failed as it was too advanced for me then.  Now I think I really understand what is happening and realized that I have a unipolar stepper when the instructables calls for what I can only assume is a 6 wire bi-polar stepper, as it uses a uln2003a(a bi-polar stepper driver).  Is there any way to get this project to work with my 4-wire unipolar stepper?  ( https://www.sparkfun.com/products/10551  ).  I assumed I would need a different stepper driver, so what should I be looking for?

  • Sign in to reply
  • Cancel

Top Replies

  • balearicdynamics
    balearicdynamics over 9 years ago in reply to gub11 +1 verified
    Gabriel, I think that you should try to find a scenario on how the stepepr motors (bipolar and unipolar) works. First of all, divide the problem in two smaller and easier problems. Just as I have done…
Parents
  • Nate1616
    0 Nate1616 over 9 years ago

    Gabriel-

    If the link is the motor you are using then you would want something similar to this driver https://www.sparkfun.com/products/12779

    I'm not sure what the project is but be aware the code would change slightly with a different setup.

     

    Nate

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gub11
    0 gub11 over 9 years ago in reply to Nate1616

    I have been reading about the driver you linked for a bit and I think I understand how to drive my stepper with it.  If you could take a look at my code I have a pretty simple question.  The only part dealing with the stepper is in between the sections where the laser turns on and off(you can just search for the word motor to see where I am talking about).  If I use the driver you linked I could set the MSx pins to HIGH the motor would move an eighth of a step each time.  So whenever I needed to move the motor I would just change the state of the step pin until I had to move the motor backwards, right?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • gub11
    0 gub11 over 9 years ago in reply to Nate1616

    I have been reading about the driver you linked for a bit and I think I understand how to drive my stepper with it.  If you could take a look at my code I have a pretty simple question.  The only part dealing with the stepper is in between the sections where the laser turns on and off(you can just search for the word motor to see where I am talking about).  If I use the driver you linked I could set the MSx pins to HIGH the motor would move an eighth of a step each time.  So whenever I needed to move the motor I would just change the state of the step pin until I had to move the motor backwards, right?