Arduino Forum control arduino with android app
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
  • State Suggested Answer
  • Replies 8 replies
  • Answers 4 answers
  • Subscribers 403 subscribers
  • Views 1875 views
  • Users 0 members are here
Related

control arduino with android app

Former Member
Former Member over 9 years ago

Hey guys.

I'm new here and new to using an Arduino.

Basically all I'm looking to do is to be able to control the pin out puts of my arduino using my android phone using the OTG cable (serial usb).

I've modified a sketch that i found online and i believe it will work, however, i do not know how to code an app to do what i want it to do. I have tried MIT App inventor but it does not seem to allow communication

over a serial link, only bluetooth and i am unsure of how to use android studio or eclipse.

My project is a simple 4 channel relay. If anyone can help or knows of an app which already exist, i would be greatful.

 

Thank you.

 

Here is the sketch that I'm using :

 

int ledpin[6] = {2,4,6,8,10,12};

int ledstate[] = {3,5,7,9,11,13};

String rx="";

byte b = 0;

char c = 'a';

boolean rx_done = false;

 

void setup(){

  pinMode(2,OUTPUT);

  pinMode(4,OUTPUT);

  pinMode(6,OUTPUT);

  pinMode(8,OUTPUT);

  pinMode(10,OUTPUT);

  pinMode(12,OUTPUT);

 

  pinMode(3,INPUT);

  pinMode(5,INPUT);

  pinMode(7,INPUT);

  pinMode(9,INPUT);

  pinMode(11,INPUT);

  pinMode(13,INPUT);

 

  Serial.begin(9600);

}

 

void loop(){

 

  while(Serial.available()){

    char c = (char) Serial.read();

    rx += c;

    delay(2);

  }

 

  if(rx != ""){

    int pin_number = rx.charAt(0)-48;

    //int pin_state = rx.charAt(1)-48;

    if(pin_number > 5){

      //Serial.println("false");

    }

    else{

      int new_state;

      if(digitalRead(ledpin[pin_number]) == HIGH){

        new_state = 0;

        digitalWrite(ledpin[pin_number],new_state);

      } else {

        new_state = 1;

        digitalWrite(ledpin[pin_number],new_state);

      }

     

      String s = rx+new_state;

      Serial.print(s);

    }

   

    rx ="";

  }

 

  delay(1000);

}

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 9 years ago +2 suggested
    If you just want to control relays from android using USB, you could check out EECI. They make the relay card and android app... USB Relay - USB Analog to Digital with Data Logger - RS-232, RS-485 Relay…
  • Former Member
    Former Member over 9 years ago in reply to balearicdynamics +1
    Thank you very much
Parents
  • neilk
    0 neilk over 9 years ago

    Hi ashman  Enrico is correct: the most reliable approach is to use Bluetooth between your Android device and your Arduino.

     

    Bluetooth adapters are readily and cheaply available - HC-06 is very easy to use.

     

    Here is a very simple example, using App Inventor:

     

    https://www.element14.com/community/people/neilk/blog/2014/07/14/mit-app-inventor-creating-android-app-to-control-arduino-via-bluetooth

     

    Hope this helps

     

    Neil

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • neilk
    0 neilk over 9 years ago

    Hi ashman  Enrico is correct: the most reliable approach is to use Bluetooth between your Android device and your Arduino.

     

    Bluetooth adapters are readily and cheaply available - HC-06 is very easy to use.

     

    Here is a very simple example, using App Inventor:

     

    https://www.element14.com/community/people/neilk/blog/2014/07/14/mit-app-inventor-creating-android-app-to-control-arduino-via-bluetooth

     

    Hope this helps

     

    Neil

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer