Arduino Forum control arduino with android app
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
  • State Suggested Answer
  • Replies 8 replies
  • Answers 4 answers
  • Subscribers 403 subscribers
  • Views 1877 views
  • Users 0 members are here
Related

control arduino with android app

Former Member
Former Member over 9 years ago

Hey guys.

I'm new here and new to using an Arduino.

Basically all I'm looking to do is to be able to control the pin out puts of my arduino using my android phone using the OTG cable (serial usb).

I've modified a sketch that i found online and i believe it will work, however, i do not know how to code an app to do what i want it to do. I have tried MIT App inventor but it does not seem to allow communication

over a serial link, only bluetooth and i am unsure of how to use android studio or eclipse.

My project is a simple 4 channel relay. If anyone can help or knows of an app which already exist, i would be greatful.

 

Thank you.

 

Here is the sketch that I'm using :

 

int ledpin[6] = {2,4,6,8,10,12};

int ledstate[] = {3,5,7,9,11,13};

String rx="";

byte b = 0;

char c = 'a';

boolean rx_done = false;

 

void setup(){

  pinMode(2,OUTPUT);

  pinMode(4,OUTPUT);

  pinMode(6,OUTPUT);

  pinMode(8,OUTPUT);

  pinMode(10,OUTPUT);

  pinMode(12,OUTPUT);

 

  pinMode(3,INPUT);

  pinMode(5,INPUT);

  pinMode(7,INPUT);

  pinMode(9,INPUT);

  pinMode(11,INPUT);

  pinMode(13,INPUT);

 

  Serial.begin(9600);

}

 

void loop(){

 

  while(Serial.available()){

    char c = (char) Serial.read();

    rx += c;

    delay(2);

  }

 

  if(rx != ""){

    int pin_number = rx.charAt(0)-48;

    //int pin_state = rx.charAt(1)-48;

    if(pin_number > 5){

      //Serial.println("false");

    }

    else{

      int new_state;

      if(digitalRead(ledpin[pin_number]) == HIGH){

        new_state = 0;

        digitalWrite(ledpin[pin_number],new_state);

      } else {

        new_state = 1;

        digitalWrite(ledpin[pin_number],new_state);

      }

     

      String s = rx+new_state;

      Serial.print(s);

    }

   

    rx ="";

  }

 

  delay(1000);

}

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 9 years ago +2 suggested
    If you just want to control relays from android using USB, you could check out EECI. They make the relay card and android app... USB Relay - USB Analog to Digital with Data Logger - RS-232, RS-485 Relay…
  • Former Member
    Former Member over 9 years ago in reply to balearicdynamics +1
    Thank you very much
Parents
  • balearicdynamics
    0 balearicdynamics over 9 years ago

    Ash please contact me by email. I have a USB monitor application to check the attached devices, the USB features and also a logging features in HTML format. I can send it to you. It somewhere on the market .ru or somewhere else but I don't remember so it is better if I send you directly the app.

     

    Enrico

     

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 9 years ago in reply to balearicdynamics

    Thank you very much my email is, apotts1310@gmail.com

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 9 years ago in reply to balearicdynamics

    Thank you very much my email is, apotts1310@gmail.com

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • balearicdynamics
    0 balearicdynamics over 9 years ago in reply to Former Member

    Fine! Tomorrow I will provide you a copy.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 9 years ago in reply to balearicdynamics

    Thank you very much