Arduino
  • Products
  • More
Arduino
Arduino Forum Fuel level sensor to protect me from myself. First Arduino project
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 11 replies
  • Answers 3 answers
  • Subscribers 418 subscribers
  • Views 1490 views
  • Users 0 members are here
  • frontpage
Related

Fuel level sensor to protect me from myself. First Arduino project

e14 Contributor
e14 Contributor over 10 years ago

Im looking for guidance with my first project.

 

Background for this project.

 

I have a 100gal diesel transfer tank in my truck. From this tank i have a small 12v pump connected to the fuel tank of my truck, i use this pump to fill my truck on long trips, or if i get into areas where i cant get to a filling station. The problem I have and the reason for this project is the pump is SLOW. That in itself isnt the problem, the problem is that i sometimes forget to turn it off, and yes i have forgot about it long enough to dump 70+ gallons of fuel on the highway ( expensive mistake)

 

Scope of this project;

 

I would like to use the fuel sender in the truck tank to turn off/interrupt power to the coil of the relay controlling the pump at a set level ie. 7/8 full. This way I can turn on the switch and if i forget to turn it off i will no longer over fill the truck.

 

Since this is my first attempt working with arduino im not really sure where to start.

 

Tomorrow morning I'll be taking some measurments of the fuel sender although im pretty sure it is resistance based.

 

So i guess the first thing i need help with is interfacing with the sending unit without adversly affecting the guage on the dash.

 

 

After this part of the project is complete Id like to also monitor the sending unit in the transfer tank so when that tank is empty ( or at some set point ie. 1/4 tank) also turn off/interrupt power to the coil of the relay controlling the pump so as not to burn the pump out from running dry.

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 10 years ago in reply to e14 Contributor +2 suggested
    jamesb128 James A simple voltage comparator circuit using an OpAmp will give you all you need. It's late and bed calls but maybe if jw0752 is still up he will have the circuit and have proved it before…
  • mcb1
    mcb1 over 10 years ago +1 suggested
    jamesb128 Welcome to the world of electronics, and Arduino. Before you start you're going to have a couple of problems. 1. The sender and guage are 12v (or 24v) which is incompatible with the 5v of the…
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to mcb1 +1
    Hi mark thanks for your reply. Im certainly not tied to using an arduino or any other microcontroller for that matter. Only reason i chose to use one is well i have it and i was looking for a starter project…
Parents
  • dougw
    0 dougw over 10 years ago

    Nice project. (But why use an arduino? it seems the pump could be interrupted directly by the level sensor - no programming needed....just a little hysteresis)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • dougw
    0 dougw over 10 years ago

    Nice project. (But why use an arduino? it seems the pump could be interrupted directly by the level sensor - no programming needed....just a little hysteresis)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer