Arduino Forum what does this code do? trying to learn the basics
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
  • State Suggested Answer
  • Replies 19 replies
  • Answers 2 answers
  • Subscribers 396 subscribers
  • Views 1343 views
  • Users 0 members are here
  • help!!
  • help!
  • basic coding
  • novice
Related

what does this code do? trying to learn the basics

the_future
the_future over 9 years ago

i think i have a good idea of what this code does i was thinking it was better to hear it from the experts

 

;assex2b.asm

     .AREA  CODE1 (ABS);

     .RADIX H;

     .ORG 1000;

      LD   SP,#1100;

      LD   A,#98;

     OUT   (03), A;

 

again:       IN A,(00);

                 AND   A,(00);

                 JP Z,again;

                 LD   A,#00;

LOOP:      OUT  (01),A;

                 CALL DELAY;

                 INC  A;

                JP LOOP;

DELAY:    PUSH AF;

                LD    D,#0FF;

DECR:     DEC D;

               JP    NZ,DECR;

               POP AF;

               RET;

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago in reply to Robert Peter Oakes +3
    the scary thing is, I have not work with this assembly code in over 40 years but it still makes sense to me and seems easy to decode the functionality....
  • D_Hersey
    D_Hersey over 9 years ago +2
    What uP is this for? Squinting at this so early, seems to have a coupla infinite loops and a redundancy.
  • clem57
    clem57 over 9 years ago +2 suggested
    This is assembler for an unknown processor. Out of context, not much can be implied. Maybe if you gave the source where it was found?
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 9 years ago

    pretty obvious what it does but as already stated, this could be homework and i'm not just going to give away the answer. I would like the poster to have a go first then I will help

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 9 years ago in reply to Robert Peter Oakes

    the scary thing is, I have not work with this assembly code in over 40 years but it still makes sense to me and seems easy to decode the functionality....

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 9 years ago in reply to Robert Peter Oakes

    hehe image the same here. I haven't done any assembler since 1993 or so.

    (oh, Peter Norton's 'Assembler for the 8086', those were the days)

    I can read the program above. I don't know for what architecture it is though.

    But the mnemonix make sense - nothing outlandish.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 9 years ago in reply to Jan Cumps

    I can even remember the . commands even though it was long ago. I can give a hint that .ORG is very important clue. PM if you know why.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 9 years ago in reply to Jan Cumps

    I can even remember the . commands even though it was long ago. I can give a hint that .ORG is very important clue. PM if you know why.

    Clem