Arduino
  • Products
  • More
Arduino
Arduino Forum I am looking for a gsm gps arduino device.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 6 replies
  • Answers 1 answer
  • Subscribers 417 subscribers
  • Views 794 views
  • Users 0 members are here
  • gprs
  • gps
  • cell phone
  • gprs/gsm
  • tracking_systems
Related

I am looking for a gsm gps arduino device.

e14 Contributor
e14 Contributor over 10 years ago

I am looking for a GPRS+GPS arduino device. I have tried one from cooking hacks and have not had much luck with it.

I have the following requirements.

 

1. must be arduino compatable

2. must work with att or verizion

3. needs to have add on antennas.

4. needs to be able to have battery backup

 

It would be nice if......

the gps and cell networked in a building/house

 

Here is a link to what i bought all ready and give you an idea of what im trying to do

https://www.cooking-hacks.com/documentation/tutorials/geolocation-tracker-gprs-gps-geoposition-sim908-arduino-raspberry-…

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    gihu

    here is a link to the discussion im having regarding the device not working.

    https://www.cooking-hacks.com/forum/viewtopic.php?f=43&t=8829&p=27850&hilit=bigmuddyfoot&sid=2b94169520b46b3ccab7312c90e4c512#p27850

     

    Here is the link to the device im using

    https://www.cooking-hacks.com/gprs-gps-quadband-module-for-arduino-sim908

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gihu
    0 gihu over 10 years ago in reply to e14 Contributor

    You could try to print also the answer from the shield:

     

    int8_t sendATcommand(char* ATcommand, char* expected_answer, unsigned int timeout){

     

        uint8_t x=0,  answer=0;

        char response[100];

        unsigned long previous;

     

        ...

         ...

    //add just before the return

        

         if (answer == 1){

              Serial.println(response);

         }else{

              Serial.print("error")

         }

     

        return answer;

    }

     

     

    Then you can see also the answer from the shield, just to know what's happening.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • gihu
    0 gihu over 10 years ago in reply to e14 Contributor

    You could try to print also the answer from the shield:

     

    int8_t sendATcommand(char* ATcommand, char* expected_answer, unsigned int timeout){

     

        uint8_t x=0,  answer=0;

        char response[100];

        unsigned long previous;

     

        ...

         ...

    //add just before the return

        

         if (answer == 1){

              Serial.println(response);

         }else{

              Serial.print("error")

         }

     

        return answer;

    }

     

     

    Then you can see also the answer from the shield, just to know what's happening.