Arduino Forum Can someone help me with some code?
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
  • State Verified Answer
  • Replies 5 replies
  • Subscribers 391 subscribers
  • Views 427 views
  • Users 0 members are here
Related

Can someone help me with some code?

Former Member
Former Member over 9 years ago

Here is what I want to do.

I want to use two of these sensors:5pcs Slot Type Optocoupler Module 3 3V 5V Counter Speed Test Sensor for Arduino | eBay

These are mounted  so they sense an encoder wheel that moves fairly slow. The encoder wheel has one slot.The sensors have both an analog and digital output and of course power(5V,gnd)

Using an arduino UNO and a 1602LCD display, I would like to be able for the arduino to count the pulses from the sensor and display the count on the LCD.

I need the count to go to 100. The LCD should have text(I.E.) shaft #1 on the first line and shaft #2 on the second followed by the actual count from

the sensors.

I would also like one pushbutton for each that resets the counts to zero to start over, and one final button that resets both counts to zero.

If this is too extensive or time consuming, perhaps enough code for a single line of the display, one counter and reset?

This is for a test rig I am making for my engine projects.

 

 

 

any help would be appreciated!

 

Thanks

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 9 years ago

    Hi Mark,

     

    somewhere in the future I would like to count the spindle revolutions on my mini-lathe to be able to cut tread without fumbling with gears.

    Your project is alike aside from the sensortypes.

    I've build a few things with Arduino, not too complicated and mostly out of curiosity.  I would be happy work with you if you wish to.

    BTW : 57 in august.  

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 9 years ago in reply to Former Member

    Marc,

    Still not working,but thanks for your help and hard work.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 9 years ago in reply to Former Member

    Marc,

    Still not working,but thanks for your help and hard work.