Arduino
  • Products
  • More
Arduino
Arduino Forum Electrical questions about my robot
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 26 replies
  • Answers 17 answers
  • Subscribers 420 subscribers
  • Views 2708 views
  • Users 0 members are here
  • arduino uno
Related

Electrical questions about my robot

braedan
braedan over 10 years ago

Hello Element14 community,

 

I have an amateur understanding of dc electronics but there are a few questions that i haven't found any other threads or discussions on. Probably because i do not know the name of the specific topic.

Forgive me if the answer is obvious, but my first question is on current placement. When i look at a solder less breadboard there are two lanes for a positive and negative voltage from a power supply. Say i have an 6v red led drawing 30ma from the power supply, but is connected to the power supply from the middle of the breadboards power lanes. Now if there is a 6v dc motor connected to the end of the power lanes and is drawing 1.5 amps or so, does the high current affect the led in front of the motor? again: there are 1.5 amps going across the power lanes to the motor at the end, but there is a small led drawing much less current before the motor from the same power source.

 

My second question is about capacitors. I have an array of Sharp (brand) Infrared distance sensors that operate at 5 volts and draw current in sharp bursts rated at around 30-60ma on average. I am planning on wiring all 37 of them to 3, 16 channel multiplexers connected to and Arduino uno that will then read the sensors analog output. (Multiplexer i will be using is the cd74hc4067). I have two questions on this topic, both of them about power connectivity. My first question is about the sensors. On a the sensors website and data sheet they both strongly recommend the use of some sort of capacitor to smooth things out. Please look at the picture attached and help me find the best places to add this extra circuitry. Please keep in mind that the S in the image is the Sharp infrared distance sensor and there are actually 37 sensors and not 3. Second is about the power it self. I was told that the sensor array would take little over 1.5 amps and to be safe i should have a power supply that can supply double the amount of current needed. The problem is that i don't actually need a power supply because i will be running this off a 12v lead acid battery. I'm not sure how to build a voltage regulator that can supply this amount of current (3 amps), if a voltage regulator is what i need. later I found this UBEC DC/DC Step-Down (Buck) Converter 5v @ 3a output on Adafruit but yet again i'm skeptical if it will properly power everything.

 

P.S. - Could a 12v 7aH lead acid battery (specifically this one: https://www.amazon.com/ExpertPower-EXP1270-Rechargeable-Lead-Battery/dp/B003S1RQ2S/ref=sr_1_3?ie=UTF8&qid=1468962932&sr=… )

power this arduino sensor array? Specifically how much am i able to draw from this battery? In the future i plan on building a large robot and i need a battery that will be able to power this sensor array, 3 sub 100watt 24v DC motors, 2 small 24v DC gear motors,a raspberry pi 2b and a 12v dc VGA monitor. I know its allot but they all wont be running at once (mainly the motors) and i also know that i can increase the battery capacity by wiring two or more together in parallel (please correct me if i'm wrong). I'm just asking if this lead acid battery type can discharge the required amount of power with out any battery problems, i don't what any battery fires or an explosion.

 

 

Please write me back and helpful links or answers to my questions!

Thank you for your time!

Attachments:
image
  • Sign in to reply
  • Cancel

Top Replies

  • DAB
    DAB over 10 years ago +3 suggested
    Hi Braedan, You have an ambitious plan and I highly suggest you find someone local to help you with the electronics. Most drive circuits use either a constant current device and or a nice capacitor bank…
  • billpenner
    billpenner over 10 years ago in reply to jw0752 +2 suggested
    just a few thoughts, Braedan: You should definitely use a buck converter for the circuits other than the motors. Since the motors will be 24 volts and other circuits will be 5 Volts, the basic power supply…
  • michaelwylie
    michaelwylie over 10 years ago +2 suggested
    Q1 - Ideally one load does not effect the other. In reality many things can happen. For instance, in your example provided, the motor, or any inductive load, will produce an EMF that will likely feedback…
Parents
  • dougw
    0 dougw over 10 years ago

    Question 1 - you won't notice the difference in LED brightness.

    Question 2 - the 3A buck converter should be able to drive all sensors. These sensors have high instantaneous spike currents, so I would put large capacitors on the power pins (at least 10 uf)

    Question 3 - the battery can run the load but will need some de-rating. Your battery is rated at 7 A-Hr when discharged over 20 hours - this is discharging at only 2.86 A. If you draw 4 times this current (11.4 A) the battery becomes a 5 A-Hr battery (lasting about 25 min) You will need heavy wire to carry this current and the battery will get pretty warm. I would monitor the battery temperature and shut down if it gets over about 50C. You don't need a circuit, just touch the battery while it is running - when it gets too hot  to touch, that tells you how long it can run before you need to cool it off. It might never get too hot if the motor is not under heavy continuous load.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • braedan
    0 braedan over 10 years ago in reply to dougw

    Thank you Douglas!

        Your response was just was I needed!

    I just have two questions:

     

    #1. When you say " large capacitor", would it be an ceramic cap or an electrolite cap? Also, would I need a cap for every sensor; a capacitor across the positive and negative lines for each individual sensor. Or a cap across the main power rail to all the sensors? Maybe I would need a combination of both?

     

    #2. Could a raspberry pi 2b run of another 3a buck converter with out damaging it Or the converter?

    Also, if the motors charge the main power line from the battery could it damage the pi? Then sensors? The battery it self? Is there some basic circuit or breakout board I could use to protect the main power line (battery) from the motors back EMF or some other damaging force from breaking other components.

     

    Thanks again - Braedan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • braedan
    0 braedan over 10 years ago in reply to dougw

    Thank you Douglas!

        Your response was just was I needed!

    I just have two questions:

     

    #1. When you say " large capacitor", would it be an ceramic cap or an electrolite cap? Also, would I need a cap for every sensor; a capacitor across the positive and negative lines for each individual sensor. Or a cap across the main power rail to all the sensors? Maybe I would need a combination of both?

     

    #2. Could a raspberry pi 2b run of another 3a buck converter with out damaging it Or the converter?

    Also, if the motors charge the main power line from the battery could it damage the pi? Then sensors? The battery it self? Is there some basic circuit or breakout board I could use to protect the main power line (battery) from the motors back EMF or some other damaging force from breaking other components.

     

    Thanks again - Braedan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • dougw
    0 dougw over 10 years ago in reply to braedan

    #1 - I think these sensors have small ceramic capacitors on-board so you only need electrolytic decoupling. It is better to have one cap at each sensor, but it will most likely be fine with a single 100 uf cap on the supply, especially if the power wires are reasonably heavy wire. Running a star wiring arrangement is better than a daisy chain, but again a daisy chain can still work. If you have problems with a minimal solution, you can always add extra caps or wire.

    #2 - yes this should work fine and it isolates the Pi from sensor current spikes (and vice versa)

    #2a - if you are running all analog and digital circuits from buck converters off the battery, motor noise or other noise on the battery shouldn't affect your sensitive circuits.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer