Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino Flora with light sensor
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 19 replies
  • Answers 6 answers
  • Subscribers 408 subscribers
  • Views 1830 views
  • Users 0 members are here
  • light sensor
  • adafruit_flora
  • neopixels
  • arduino
Related

Arduino Flora with light sensor

Former Member
Former Member over 9 years ago

Hello all.  I am VERY new at Arduino coding, and I am trying to get my Flora and Neopixels to respond using the light sensor.  Something is wrong with my code, and no matter how I try to adjust it, I am still getting errors.  Any help would be appreciated....

And I apologize, but I don't know how to put code tags. 

 

The errors I am getting are the following:

 

(sketch file) light sensor.ino:162:5: error: use of undeclared identifier 'colorWipe'

  colorWipe(strip.Color(255,250,240));

  ^
(sketch file) light sensor.ino:167:5: error: use of undeclared identifier 'colorWipe'

  colorWipe(strip.Color(0,255,0));

  ^
(sketch file) light sensor.ino:172:5: error: use of undeclared identifier 'colorWipe'

  colorWipe(strip.Color(255,0,0));

 

My code so far:

 

#include <Wire.h>

#include <Adafruit_Sensor.h>

#include <Adafruit_TSL2561_U.h>

#include <Adafruit_NeoPixel.h>

 

 

#define PIN 6

Adafruit_NeoPixel strip = Adafruit_NeoPixel(4, PIN, NEO_GRB + NEO_KHZ800);

 

 

 

 

 

 

/* This driver uses the Adafruit unified sensor library (Adafruit_Sensor),

   which provides a common 'type' for sensor data and some helper functions.

  

   To use this driver you will also need to download the Adafruit_Sensor

   library and include it in your libraries folder.

   You should also assign a unique ID to this sensor for use with

   the Adafruit Sensor API so that you can identify this particular

   sensor in any data logs, etc.  To assign a unique ID, simply

   provide an appropriate value in the constructor below (12345

   is used by default in this example).

  

   Connections

   ===========

   Connect SCL to analog 5

   Connect SDA to analog 4

   Connect VDD to 3.3V DC

   Connect GROUND to common ground

   I2C Address

   ===========

   The address will be different depending on whether you leave

   the ADDR pin floating (addr 0x39), or tie it to ground or vcc.

   The default addess is 0x39, which assumes the ADDR pin is floating

   (not connected to anything).  If you set the ADDR pin high

   or low, use TSL2561_ADDR_HIGH (0x49) or TSL2561_ADDR_LOW

   (0x29) respectively.

   

   History

   =======

   2013/JAN/31  - First version (KTOWN)

*/

  

Adafruit_TSL2561_Unified tsl = Adafruit_TSL2561_Unified(TSL2561_ADDR_FLOAT, 12345);

 

 

/**************************************************************************/

/*

    Displays some basic information on this sensor from the unified

    sensor API sensor_t type (see Adafruit_Sensor for more information)

*/

/**************************************************************************/

void displaySensorDetails(void)

{

  sensor_t sensor;

  tsl.getSensor(&sensor);

  Serial.println("------------------------------------");

  Serial.print  ("Sensor:       "); Serial.println(sensor.name);

  Serial.print  ("Driver Ver:   "); Serial.println(sensor.version);

  Serial.print  ("Unique ID:    "); Serial.println(sensor.sensor_id);

  Serial.print  ("Max Value:    "); Serial.print(sensor.max_value); Serial.println(" lux");

  Serial.print  ("Min Value:    "); Serial.print(sensor.min_value); Serial.println(" lux");

  Serial.print  ("Resolution:   "); Serial.print(sensor.resolution); Serial.println(" lux"); 

  Serial.println("------------------------------------");

  Serial.println("");

  delay(500);

}

 

 

/**************************************************************************/

/*

    Configures the gain and integration time for the TSL2561

*/

/**************************************************************************/

void configureSensor(void)

{

  /* You can also manually set the gain or enable auto-gain support */

  // tsl.setGain(TSL2561_GAIN_1X);      /* No gain ... use in bright light to avoid sensor saturation */

  // tsl.setGain(TSL2561_GAIN_16X);     /* 16x gain ... use in low light to boost sensitivity */

  tsl.enableAutoRange(true);            /* Auto-gain ... switches automatically between 1x and 16x */

 

  /* Changing the integration time gives you better sensor resolution (402ms = 16-bit data) */

  tsl.setIntegrationTime(TSL2561_INTEGRATIONTIME_13MS);      /* fast but low resolution */

  // tsl.setIntegrationTime(TSL2561_INTEGRATIONTIME_101MS);  /* medium resolution and speed   */

  // tsl.setIntegrationTime(TSL2561_INTEGRATIONTIME_402MS);  /* 16-bit data but slowest conversions */

 

 

  /* Update these values depending on what you've set above! */ 

  Serial.println("------------------------------------");

  Serial.print  ("Gain:         "); Serial.println("Auto");

  Serial.print  ("Timing:       "); Serial.println("13 ms");

  Serial.println("------------------------------------");

}

 

 

 

 

 

 

/**************************************************************************/

/*

    Arduino setup function (automatically called at startup)

*/

/**************************************************************************/

void setup(void)

{

  Serial.begin(9600);

  Serial.println("Light Sensor Test"); Serial.println("");

 

  /* Initialise the sensor */

  if(!tsl.begin())

  {

    /* There was a problem detecting the ADXL345 ... check your connections */

    Serial.print("Ooops, no TSL2561 detected ... Check your wiring or I2C ADDR!");

    while(1);

  }

 

  /* Display some basic information on this sensor */

  displaySensorDetails();

 

  /* Setup the sensor gain and integration time */

  configureSensor();

 

  /* We're ready to go! */

  Serial.println("");

  

    // This is for Trinket 5V 16MHz, you can remove these three lines if you are not using a Trinket

  #if defined (__AVR_ATtiny85__)

    if (F_CPU == 16000000) clock_prescale_set(clock_div_1);

  #endif

  // End of trinket special code

 

 

 

 

  strip.begin();

  strip.show(); // Initialize all pixels to 'off'

}

 

 

 

 

/**************************************************************************/

/*

    Arduino loop function, called once 'setup' is complete (your own code

    should go here)

*/

/**************************************************************************/

void loop(void)

{

 

 

  /* Get a new sensor event */

  sensors_event_t event;

  tsl.getEvent(&event);

 

  /* Display the results (light is measured in lux) */

  if (event.light)

  {

    Serial.print(event.light); Serial.println(" lux");

  }

  else

  {

    /* If event.light = 0 lux the sensor is probably saturated

       and no reliable data could be generated! */

    Serial.println("Sensor overload");

  }

  delay(250);

 

 

 

 

 

  //>130 is (255, 250, 240)

if (event.light > 130)

{

    colorWipe(strip.Color(255,250,240));

}

// 129-50 is (0,255,0)

else if ((event.light > 50) && (event.light < 129))

{

    colorWipe(strip.Color(0,255,0));

}

// and <50 is (255, 0, 0)

else if (event.light < 50)

{

    colorWipe(strip.Color(255,0,0));

}

 

 

}

  • Sign in to reply
  • Cancel

Top Replies

  • Former Member
    Former Member over 9 years ago +3
    Hey Jennifer, just for future reference, it would be easier if you just copy-pasted the link to your codebender project so that others can look at the code in an easier way, and even compile it to look…
  • Former Member
    Former Member over 9 years ago in reply to mcb1 +3
    yeah sure, i'm not saying it's the only way, or the "right" way, I'm just saying this helps a lot of back and forth questions of "which library version are you using", "do you have that installed", "ok…
  • Former Member
    Former Member over 9 years ago in reply to Former Member +2
    IT'S WORKING!!! I don't know exactly what I did, but thank you all soooo much! mcb1, you are awesome!!! I am completely thrilled, because now I know where I can change things on this code to be able to…
Parents
  • Former Member
    0 Former Member over 9 years ago

    Hey Jennifer,

    just for future reference, it would be easier if you just copy-pasted the link to your codebender project so that others can look at the code in an easier way, and even compile it to look at the exact errors you're getting image

     

    As it happens, I am the co-founder of codebender image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 9 years ago in reply to Former Member

    if you just copy-pasted the link to your codebender project

    tzikis

    While it might suit some people, it wouldn't be very useful for anyone else using this website.

    If for any reason the link got broken then someone searching for an answer to a similar problem might not be able to follow it.

     

    It would also mean I would then have to cut and paste from the link to answer the query.

    (Assumming I even bother to follow the link ..)

     

    This has been a great learning experience for jbarker822 and hopefully has helped unravel some of the mysteries.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 9 years ago in reply to mcb1

    yeah sure, i'm not saying it's the only way, or the "right" way, I'm just saying this helps a lot of back and forth questions of "which library version are you using", "do you have that installed", "ok it worked but now I get this error" etc. you just click on the link, click compile, see the error, fiddle with it till it works, and there you have it

     

    there's definitely advantages and disadvantages for each, as with most things

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 9 years ago in reply to mcb1

    yeah sure, i'm not saying it's the only way, or the "right" way, I'm just saying this helps a lot of back and forth questions of "which library version are you using", "do you have that installed", "ok it worked but now I get this error" etc. you just click on the link, click compile, see the error, fiddle with it till it works, and there you have it

     

    there's definitely advantages and disadvantages for each, as with most things

    • Cancel
    • Vote Up +3 Vote Down