Arduino Forum I want to build one-to-one wireless system with arduino nano and NRF24l01 and RF24
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
  • State Suggested Answer
  • Replies 1 reply
  • Answers 1 answer
  • Subscribers 401 subscribers
  • Views 351 views
  • Users 0 members are here
  • audio
  • wirelessreceiver
  • wirelesstransmitter
  • wireless
  • nrf24l01
  • arduino
Related

I want to build one-to-one wireless system with arduino nano and NRF24l01 and RF24

tomstr21
tomstr21 over 9 years ago

I want to build one-to-one wireless audio system using NRF24l01 and NRF24Audio library and I came across this example which looks right http://arduino.cc/en/Tutorial/InputPullupSerial  but here they say something about connecting the operating buttons to analog pins on arduino and that doesn't feel right to me but as I'm not so experienced with arduino i wanted to ask someone who will maybe help me with this..

 

P.S: also you have to set a radio number--if I want to have one-to-one the numbers on the two arduinos will be set the same?!

 

 

Thanks,

Tomas

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago +2 suggested
    Analog pins work perfectly well as Digital pins, just initialize them as you would a digital pin and away you go. The chip supports multiple uses for most of its pins. for instance A4 and A5 also double…
  • Robert Peter Oakes
    0 Robert Peter Oakes over 9 years ago

    Analog pins work perfectly well as Digital pins, just initialize them as you would a digital pin and away you go. The chip supports multiple uses for most of its pins. for instance A4 and A5 also double up as the I2C (Digital) serial bus interface. Digital pins 10,11,12,13 also function as the SPI interface, many other pins can be PWM outputs.

     

    Hope this helps

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer