Arduino Forum Making toggle switch work in game
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
  • State Verified Answer
  • Replies 4 replies
  • Subscribers 392 subscribers
  • Views 928 views
  • Users 0 members are here
  • code
  • toggle_switch
Related

Making toggle switch work in game

pot82es
pot82es over 9 years ago

Hi, I just got the Arduino micro, and I'm very bad at writing code...

I found this code down below at http://forum.arduino.cc/index.php?topic=121129.0

 

My problem is that when I press the toggle switch it just spits out G's with 100ms delay, and stops when I turn the toggle switch off. My goal is to make it write a G only once on my computer when the toggle switch is pressed on or off (changing state). This way I can make a toggle switch that retracts a landing gear ingame whenever its pressed. I do not know what to do next... I'm hoping anyone have a solution. Thanks.

 

GIF by silviustro

 

image

 

#include <Keyboard.h>

boolean toggleState; // hold current state of switch

boolean lastToggleState;  // hold last state to sense when switch is changed

long toggleTimer = millis();  // // debounce timer

const int toggleSwitchPin = 9;

 

 

 

 

void setup(){

// setup stuff here

}

 

 

void loop(){

 

 

toggleState = digitalRead(toggleSwitchPin);

 

 

if (millis() - toggleTimer > 100){  // debounce switch 100ms timer

  if (toggleState && !lastToggleState) {  // if switch is on but was previously off

    lastToggleState = true;  // switch is now on

    toggleTimer = millis();  // reset timer

    Keyboard.write('G');

  }

 

 

  if (!toggleState && lastToggleState){  // if switch is off but was previously on

    lastToggleState = false; // switch is now off

    toggleTimer = millis(); // reset timer

    }

  }

}

 

Code is originally written by

Goofballtech

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago +1
    Your answer is a few post down from the one your code came from Toggle switch act like a button?
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 9 years ago

    Your answer is a few post down from the one your code came from image

    Toggle switch act like a button?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • pot82es
    0 pot82es over 9 years ago in reply to Robert Peter Oakes

    Ok, but I do not understand how, in his example it says do stuff here on both, so i set keyboard write on both. Could u give me an example?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • pot82es
    0 pot82es over 9 years ago in reply to Robert Peter Oakes

    Ok, but I do not understand how, in his example it says do stuff here on both, so i set keyboard write on both. Could u give me an example?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Robert Peter Oakes
    0 Robert Peter Oakes over 9 years ago in reply to pot82es

    If you look at your first code sample, it has initialization stuff in setup, thats what needs to go into the setup() block in this one. the poster just did not repeat obvious stuff.

     

    In the loop() structures you add the code to write the "G" to the serial ports etc,

     

    if you look at the two posts you will see the difference, this post simply shows the code needed to handle the non repeating output to the serial port

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • pot82es
    0 pot82es over 9 years ago in reply to Robert Peter Oakes

    Thank you, I believe got it image