Arduino Forum Trigger LED if 3 sensores are triggered in a specific order
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
  • State Not Answered
  • Replies 1 reply
  • Subscribers 391 subscribers
  • Views 243 views
  • Users 0 members are here
Related

Trigger LED if 3 sensores are triggered in a specific order

hafizbilal
hafizbilal over 8 years ago

Looking for Arduino project using 3 light sensors when the sensors are shined on with a laser in the correct order a green led will turn on for 5 seconds and trigger a relay if the wrong order is done a red light flashes for 10 seconds then the game resets. need code

  • Sign in to reply
  • Cancel
Parents
  • ravi_butani
    0 ravi_butani over 8 years ago

    Well you can interface LDR directly on Analog Input Pins of Arduino with only simple voltage divider network, No need to use opamp/comperators...

    as far as program is concern.... you need one more input to trig program to record sequence of events on sensors...otherwise order/sequence 123,231,321 is same and 132,321,213 is same...

     

    Hope it helps,

     

    Ravi

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ravi_butani
    0 ravi_butani over 8 years ago

    Well you can interface LDR directly on Analog Input Pins of Arduino with only simple voltage divider network, No need to use opamp/comperators...

    as far as program is concern.... you need one more input to trig program to record sequence of events on sensors...otherwise order/sequence 123,231,321 is same and 132,321,213 is same...

     

    Hope it helps,

     

    Ravi