Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Did i code brick my Arduino uno?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 3 replies
  • Answers 2 answers
  • Subscribers 417 subscribers
  • Views 1112 views
  • Users 0 members are here
  • arduino uno
  • bricked
Related

Did i code brick my Arduino uno?

supper_slash
supper_slash over 10 years ago

Arduino no longer shows up on a COM port.

 

I am working on a 200khz 50% waveform generator.

 

I was working on a sketch and then running the arduino over to my scope to find out where I am at.

I managed to get it to 250khz with this sketch and all was well.

 

#include <avr/io.h>
#include <util/delay.h>


int main(void)
{
  pinMode(3, OUTPUT); // output pin for OCR2B
  pinMode(5, OUTPUT); // output pin for OCR0B


  // Set up the 250KHz output
  TCCR2A = _BV(COM2A1) | _BV(COM2B1) | _BV(WGM21) | _BV(WGM20);
  TCCR2B = _BV(WGM22) | _BV(CS20);
  OCR2A = 63;  //This is the reset point out of 255 count setting the frequency to 200khz.
  //The higher the number in "OCR2A" the lower the Frequency.


  OCR2B = 0;  //This sets the duration of the pulse, half of the above number is = to 50% on time.
}
// Set up 8MHz output
//TCCR0A = _BV(COM0A1) | _BV(COM0B1) | _BV(WGM01) | _BV(WGM00);
//TCCR0B = _BV(WGM02) | _BV(CS00);
//OCR0A = 1;
//OCR0B = 0;


// Make the 250KHz rolling
//while (1) {
//_delay_us(5);
// if ( OCR2B < 63 )
// OCR2B += 5;
// else
//   OCR2B = 0;
// }
//}

 

It was working fine, I plugged it back in and changed line 14, to: "OCR2A = 51;  //This is the reset point out of 255 count setting the frequency to 200kHz.".

And line 18 to "OCR2B = 26;  //This sets the duration of the pulse, half of the above number is = to 50% on time.".

 

And now the led's light up on the board, but there is no out put on any pins. Also when I reconnect it to the USB, it will not show up on any com port...

I am running win 10, and I tried another Arduino on the same cord, and USB port and it works fine. I shows up on com4.

So before I try and upload this code to the new board does anyone see anything in the code that can harm the arduino?

imageimage

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 10 years ago +2 suggested
    The USB connetivity should be done via the USB chip, rather than the Atmel 328 chip. Three questions. Does it show in whatever operating system you are using as a connected device (ignore the Arduino IDE…
  • clem57
    clem57 over 10 years ago +1
    The code did not brick the Uno. But if the boot-loader is gone(?), you can use the other working Uno to load a new boot-loader to the bad Uno. Try that and see if the Uno works again. Clem
Parents
  • clem57
    0 clem57 over 10 years ago

    The code did not brick the Uno. But if the boot-loader is gone(?), you can use the other working Uno to load a new boot-loader to the bad Uno. Try that and see if the Uno works again.

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 10 years ago

    The code did not brick the Uno. But if the boot-loader is gone(?), you can use the other working Uno to load a new boot-loader to the bad Uno. Try that and see if the Uno works again.

    Clem