Arduino Forum How can connect multi vibrator motors with arduino Uno?
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
  • State Suggested Answer
  • Replies 5 replies
  • Answers 4 answers
  • Subscribers 402 subscribers
  • Views 1188 views
  • Users 0 members are here
Related

How can connect multi vibrator motors with arduino Uno?

manisha17
manisha17 over 9 years ago

I want to know the interfacing and coding for connection of multi vibrator motors with arduino Uno....plzz help me out...

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 9 years ago +3 suggested
    Hi Manisha, You will have to give more information about what you want to do and show us the work you have put into this project already. As it sits your question merits an answer like: Connect the wires…
  • dougw
    dougw over 9 years ago in reply to manisha17 +2 suggested
    Is there other functionality required? (It doesn't seem like you need an arduino - the motors could be directly controlled by the sensors.) John Wiltrout's Blog built such a system here: Automatic Water…
Parents
  • jw0752
    0 jw0752 over 9 years ago

    Hi Manisha,

     

    You will have to give more information about what you want to do and show us the work you have put into this project already. As it sits your question merits an answer like:

     

    Connect the wires up properly and put the code in proper sequence and everything will work as planned.

     

    I hope to be able to contribute more appropriately to a more concise question.

     

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 9 years ago

    Hi Manisha,

     

    You will have to give more information about what you want to do and show us the work you have put into this project already. As it sits your question merits an answer like:

     

    Connect the wires up properly and put the code in proper sequence and everything will work as planned.

     

    I hope to be able to contribute more appropriately to a more concise question.

     

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • manisha17
    0 manisha17 over 9 years ago in reply to jw0752

    hello sir,

    Thanks for reply.....

    I want to integrate water sensor with vibration motors means water sensor detects water and then vibration motors notify the user about water detection.So i want to know exact code for this by which I can correct my errors.

     

    Manisha

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 9 years ago in reply to manisha17

    Hi Manisha,

    Do you have the parts that you intend to use? The first step is to hookup the water sensor and test to see that it is working and sensing as you expect. To begin with I would probably use an LED for the output instead of a vibration motor. Once you have the water sensor working correctly you can replace the LED with one of the circuits that Doug gave you up above. It is probably a good idea to have the Arduino turn on a MOSFET and then have the MOSFET turn on the motors. Don't forget to put a protection diode in the circuit to protect the MOSFET. You may find good support information for the water sensor from where ever you purchase it. If not then a search of the web will usually turn u some hookup information. Coding will need to be done to get the Arduino to read the input from the sensor and then to turn on the motor under the conditions that you program for. Once you have the project started and under test yu will be able to post pictures and schematics to assist us in answering specific questions.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • dougw
    0 dougw over 9 years ago in reply to manisha17

    Is there other functionality required? (It doesn't seem like you need an arduino - the motors could be directly controlled by the sensors.)

    John Wiltrout's Blog built such a system here:

    Automatic Water Shut Off System for the Home Chapter I

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer