Arduino Forum Build Amazing Speaker
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
  • State Not Answered
  • Replies 5 replies
  • Subscribers 402 subscribers
  • Views 569 views
  • Users 0 members are here
  • noise cancellation
  • digital signal processing
  • speaker amplifier
  • visual eq
  • speaker
Related

Build Amazing Speaker

abolfazlnejatian
abolfazlnejatian over 9 years ago

Hey everyone

I’m gonna build up a PC speaker with Arduino, and my desired speaker detailed as follows:

  1. 3.5 mm jack, Bluetooth and USB as an input section.
  2. I need to make some process on my input signal (FFT and cross-correlation) in order to create visual EQ on LCD, Reinforcing/Weakening some signal’s frequency in case of need and pass signal throw an adaptive noise cancellation like RLS (or LMS algorithm in the case of memory shortage) and a vocal commander, turn on/down volume, next/previous and pause/stop command with voice command.(it’s totally depend on the processing speed and memory, I doubt Arduino can handle it image)
  3. And in output section, two approximately 60 Watt speakers (I don’t know which one is more accurate!!! two mono amplifier or one stereo amplifier.)

So gimme your point of views about it and its Strengths/weak points.

I did a lot of DSP works in MATLAB environment and I know about the basis of signal processing but I don’t know about the feasibility of run it on Arduino(maybe due or mega can deal with it)

And would you please recommend your intended modules for section one and three of my question.

  • Sign in to reply
  • Cancel
Parents
  • dougw
    0 dougw over 9 years ago

    Maybe an ARM Cortex M7 has enough capability although a Cortex A7 with NEON may be better:

    NUCLEO-F746ZG STMICROELECTRONICS, Development Board, STM32F746ZG Arduino/mbed Nucleo, ST-LINK/V2-1 Debugger/Programmer |…

    32F746GDISCOVERY - Discovery kit with STM32F746NG MCU - STMicroelectronics

     

    Or an arduino DUE:

    https://www.youtube.com/watch?v=a_flWeIdoBg

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dougw
    0 dougw over 9 years ago

    Maybe an ARM Cortex M7 has enough capability although a Cortex A7 with NEON may be better:

    NUCLEO-F746ZG STMICROELECTRONICS, Development Board, STM32F746ZG Arduino/mbed Nucleo, ST-LINK/V2-1 Debugger/Programmer |…

    32F746GDISCOVERY - Discovery kit with STM32F746NG MCU - STMicroelectronics

     

    Or an arduino DUE:

    https://www.youtube.com/watch?v=a_flWeIdoBg