Arduino Forum Build Amazing Speaker
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
  • State Not Answered
  • Replies 5 replies
  • Subscribers 402 subscribers
  • Views 558 views
  • Users 0 members are here
  • noise cancellation
  • digital signal processing
  • speaker amplifier
  • visual eq
  • speaker
Related

Build Amazing Speaker

abolfazlnejatian
abolfazlnejatian over 9 years ago

Hey everyone

I’m gonna build up a PC speaker with Arduino, and my desired speaker detailed as follows:

  1. 3.5 mm jack, Bluetooth and USB as an input section.
  2. I need to make some process on my input signal (FFT and cross-correlation) in order to create visual EQ on LCD, Reinforcing/Weakening some signal’s frequency in case of need and pass signal throw an adaptive noise cancellation like RLS (or LMS algorithm in the case of memory shortage) and a vocal commander, turn on/down volume, next/previous and pause/stop command with voice command.(it’s totally depend on the processing speed and memory, I doubt Arduino can handle it image)
  3. And in output section, two approximately 60 Watt speakers (I don’t know which one is more accurate!!! two mono amplifier or one stereo amplifier.)

So gimme your point of views about it and its Strengths/weak points.

I did a lot of DSP works in MATLAB environment and I know about the basis of signal processing but I don’t know about the feasibility of run it on Arduino(maybe due or mega can deal with it)

And would you please recommend your intended modules for section one and three of my question.

  • Sign in to reply
  • Cancel
Parents
  • michaelkellett
    0 michaelkellett over 9 years ago

    I think Douglas' suggestion of the Nucleo board with a Cortex M7 is good.

    You could consider applying for the RoadTest of the TI Delfino board, although it isn't really intended for audio work.

    The best processors for serious Audio DSP are probably from Analog Devices and TI - the development tools are more expensive than for Cortex type micros.

     

    You would still need high quality DACs to drive the amplifiers.

     

    The system you are describing would represent many man-years of work and I doubt if it can be made by simple assembling of open source components.

     

    If I were you I'd start by defining what I want - is it meant to sound good or have lots of 'features' ?

     

    If good sound then don't use 3.5mm jacks,  Bluetooth, USB or digital sound ruining.

     

    If you want features - use a PC.

     

    If you want fun and to learn stuff - use the Nucleo with Cortex M7

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett over 9 years ago

    I think Douglas' suggestion of the Nucleo board with a Cortex M7 is good.

    You could consider applying for the RoadTest of the TI Delfino board, although it isn't really intended for audio work.

    The best processors for serious Audio DSP are probably from Analog Devices and TI - the development tools are more expensive than for Cortex type micros.

     

    You would still need high quality DACs to drive the amplifiers.

     

    The system you are describing would represent many man-years of work and I doubt if it can be made by simple assembling of open source components.

     

    If I were you I'd start by defining what I want - is it meant to sound good or have lots of 'features' ?

     

    If good sound then don't use 3.5mm jacks,  Bluetooth, USB or digital sound ruining.

     

    If you want features - use a PC.

     

    If you want fun and to learn stuff - use the Nucleo with Cortex M7

     

    MK