Arduino Forum Build Amazing Speaker
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
  • State Not Answered
  • Replies 5 replies
  • Subscribers 402 subscribers
  • Views 558 views
  • Users 0 members are here
  • noise cancellation
  • digital signal processing
  • speaker amplifier
  • visual eq
  • speaker
Related

Build Amazing Speaker

abolfazlnejatian
abolfazlnejatian over 9 years ago

Hey everyone

I’m gonna build up a PC speaker with Arduino, and my desired speaker detailed as follows:

  1. 3.5 mm jack, Bluetooth and USB as an input section.
  2. I need to make some process on my input signal (FFT and cross-correlation) in order to create visual EQ on LCD, Reinforcing/Weakening some signal’s frequency in case of need and pass signal throw an adaptive noise cancellation like RLS (or LMS algorithm in the case of memory shortage) and a vocal commander, turn on/down volume, next/previous and pause/stop command with voice command.(it’s totally depend on the processing speed and memory, I doubt Arduino can handle it image)
  3. And in output section, two approximately 60 Watt speakers (I don’t know which one is more accurate!!! two mono amplifier or one stereo amplifier.)

So gimme your point of views about it and its Strengths/weak points.

I did a lot of DSP works in MATLAB environment and I know about the basis of signal processing but I don’t know about the feasibility of run it on Arduino(maybe due or mega can deal with it)

And would you please recommend your intended modules for section one and three of my question.

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 9 years ago

    Would you put a Volkswagen engine in a Tesla car to save money and expect the same performance as the original car? That is the problem with the Arduino!

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 9 years ago in reply to clem57

    Would you put a Volkswagen engine in a Tesla car

    Might improve long term reliability ...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mcb1
    0 mcb1 over 9 years ago in reply to clem57

    Would you put a Volkswagen engine in a Tesla car

    Might improve long term reliability ...