Arduino Forum Automatic Timed Servo
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
  • State Suggested Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 392 subscribers
  • Views 640 views
  • Users 0 members are here
Related

Automatic Timed Servo

jasminemparham
jasminemparham over 8 years ago

I just found out today that I should add an RTC from another website comment sent to me http://www.robotshop.com/blog/en/arduino-5-minute-tutorials-lesson-5-servo-motors-3636 , because I am making my servo function on set times of the day. This will only be moving a light switch up 20 degrees then down -20 degrees. Originally I was going to convert all set hours into milli secs, which I tested. I set it to go off after a couple of minutes to see if it would work and it did, but that might mess up my order everyday for the hours i want it set on.Would you Robert Peter Oakes suggest getting the RTC? I also just made this account a couple of hrs ago today so I don`t know how to communicate to people on here.

  • Sign in to reply
  • Cancel

Top Replies

  • clem57
    clem57 over 8 years ago +1 suggested
    It is true you could use a RTC for time of day functions. Alternatively, you could get a wired/wireless connection to the internet and use a function called NTP to get the time of day functions or a website…
  • clem57
    0 clem57 over 8 years ago

    It is true you could use a RTC for time of day functions. Alternatively, you could get a wired/wireless connection to the internet and use a function called NTP to get the time of day functions or a website like Colorado time and measurements to take care of drift and daylight savings changes also.

    Just a thought,

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jasminemparham
    0 jasminemparham over 8 years ago in reply to clem57

    Thank you Clem I will test out the RTC just ordered it yesterday, and I looked into the wired/wireless connection. But I cant tell if this is a piece or a coding that can be uploaded?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 8 years ago in reply to jasminemparham

    Both hardware to connect and software to build page to get data.

    Clem