Arduino Forum detect nrf24l01 has finished transmitting
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
  • State Not Answered
  • Replies 0 replies
  • Subscribers 390 subscribers
  • Views 165 views
  • Users 0 members are here
  • wireless comunication
  • nrf24l01+
  • arduino
Related

detect nrf24l01 has finished transmitting

billpenner
billpenner over 8 years ago

I have a working project using the nRF24l01 that sends a numeric sequence to another nRF24l01. currently, the code locks up if the nRF24l01  has a problem (interference, power supply etc. . I assume that the library is requiring the nRF24l01 to acknowledge and won't continue without it. I could write code to re-transmit the data but since it is locked up I don't have the opportunity to recover. what is happening with the nRF24l01? Cna anyone help? the section of code relating to the transmitting...

ps. I think I would also like to receive an acknowledgement from the receiver but I don't know how.

 

/////////////////Transmit to wireless //////

void Xmit()            //start ......function Xmit......

{

  xmitValue = xmitValue += timeOn ; //add display time

    dataTransmitted = (xmitValue.toInt()) ;// string to int

    lcd.clear();

    lcd.setCursor(5, 0); 

    lcd.print(" DONE");

    //lcd.setCursor(0, 1);  //  option  

    //lcd.print(" Going to Sleep");  // option

    nRFRadio.write( &dataTransmitted, 5); // Transmit the data

    // Serial.print(dataTransmitted); //testing...

    delay(3000) ; //wait after transmission to clear display

    lcd.clear();

    //lcd.setBacklight(LOW) ; //blank display?.. option

}       //end ......function Xmit.....

 

I hope this makes sense.

Bill