Arduino
  • Products
  • More
Arduino
Arduino Forum Peltier on Arduino Nano
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 2 answers
  • Subscribers 418 subscribers
  • Views 1350 views
  • Users 0 members are here
Related

Peltier on Arduino Nano

alienozi
alienozi over 9 years ago

Hello fellow element14 users,

I'm making a school project with peltier modules, calculating their temparatures and shutting them down whrçen they exceed the limit temparature.

However, if I want to use peltier modules, 5V is an ideal voltage but ardunio gives 3V on its pins.

I require some help on this.

 

-Arduino Nano

-12V limV Peltier

-Temp sensor

 

I might need some help so, If we can connect using Skype or etc. It would be awesome.

 

Best regards. Oguz Alp

image

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 9 years ago +2 suggested
    Hi Oguz, You will need to get some N Channel MOSFETs that will turn on with logic level signals (3.3 Volts in this case). You can then use the MOSFETs to control 5 volts or 12 volts to your peltier modules…
  • jw0752
    jw0752 over 9 years ago in reply to alienozi +2 suggested
    I did a little research on the MOSFET RFP 30N06 used in the link I gave you above and it would be an excellent choice for load voltages up to 60 Volts. Here is a link to more information from Newark Electronics…
Parents
  • jw0752
    0 jw0752 over 9 years ago

    Hi Oguz,

    You will need to get some N Channel MOSFETs that will turn on with logic level signals (3.3 Volts in this case). You can then use the MOSFETs to control 5 volts or 12 volts to your peltier modules. You can search the internet for more examples but here is one showing how to hook up the circuit.

     

    http://bildr.org/2012/03/rfp30n06le-arduino/

     

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • alienozi
    0 alienozi over 9 years ago in reply to jw0752

    Thank you John, this will greatly acclerate the project.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • alienozi
    0 alienozi over 9 years ago in reply to jw0752

    Thank you John, this will greatly acclerate the project.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • jw0752
    0 jw0752 over 9 years ago in reply to alienozi

    I did a little research on the MOSFET RFP 30N06 used in the link I gave you above and it would be an excellent choice for load voltages up to 60 Volts. Here is a link to more information from Newark Electronics where they sell them for a little over $1 US each.

     

    http://www.newark.com/vishay/irlz34pbf/n-channel-mosfet-60v-30a-to-220/dp/63J7707?ost=RFP30N06&selectedCategoryId=&isexcsku=false&categoryNameResp=All%2BCategories&searchView=table&rpsku=rel3%3ARFP30N06LE

     

    You can also get a data sheet on this site by clicking on the Data Sheet PDF link. This MOSFET will turn on with about 2 volts which is well withing the capabilities of your Arduino. If you use any type of inductive device as a load be certain to put a flyback diode across it to prevent damage to other components in the circuit. A Peltier has minimal inductance so a diode will not be necessary with them.

     

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer