Arduino Forum Measure elevator speed
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
  • State Suggested Answer
  • Replies 5 replies
  • Answers 3 answers
  • Subscribers 404 subscribers
  • Views 780 views
  • Users 0 members are here
  • elevator
  • accelerometer
  • data set
  • arduino
  • newbie
Related

Measure elevator speed

popupideas
popupideas over 9 years ago

hi,  newbie to arduino buildouts. I was wondering if anyone could point me toward tutorials on something like the following:

i am looking to build a kit that would allow me to measure the starting acceleration, deceleration, and speed of an elevator (up and down). I have a pretty good idea of the hardware buildout but the parsing of the accelerometer data is where I think I am lost.  I believe there are formulas for calculting (while taking into account gravity). Most of the tutorials stop at showing the stream of incoming data. I hope the grab the relevant bits, calculate and display the results.

 

i saw the simplelink Texas Instruments device...not sure if that is worth while or still just raw data.

 

Any my help would be appreciated.

 

thanks

chris

  • Sign in to reply
  • Cancel
Parents
  • jw0752
    0 jw0752 over 9 years ago

    Hi Chris,

    If you are able to measure the acceleration and the time of acceleration accurately you will be able to calculate the velocity. Velocity = 1/2 Acceleration times Time Squared. The velocity itself will not be able to be measured using an accelerometer as once the elevator stops accelerating you will have no external reference point. 2 meters per second will feel exactly like 20 meters per second. If you are interested in speed of travel and where you are in the elevator shaft an accurate altimeter coupled to a time base will also work. Instead of measuring the change in distance with respect to time you will be measuring the change in air pressure with respect to time and the air pressure compared to the ground floor. Using the proper conversion formulas this data can be changed to meters per second and subsequently to distance traveled. Another challenge using acceleration is that it is not likely to be linear and you will have to integrate the change in acceleration over time to get an accurate velocity.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 9 years ago

    Hi Chris,

    If you are able to measure the acceleration and the time of acceleration accurately you will be able to calculate the velocity. Velocity = 1/2 Acceleration times Time Squared. The velocity itself will not be able to be measured using an accelerometer as once the elevator stops accelerating you will have no external reference point. 2 meters per second will feel exactly like 20 meters per second. If you are interested in speed of travel and where you are in the elevator shaft an accurate altimeter coupled to a time base will also work. Instead of measuring the change in distance with respect to time you will be measuring the change in air pressure with respect to time and the air pressure compared to the ground floor. Using the proper conversion formulas this data can be changed to meters per second and subsequently to distance traveled. Another challenge using acceleration is that it is not likely to be linear and you will have to integrate the change in acceleration over time to get an accurate velocity.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer