Arduino Forum Need Hardware list for 5-Dot-Matrix printing with Wifi-Modules
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
  • State Not Answered
  • Replies 0 replies
  • Subscribers 390 subscribers
  • Views 221 views
  • Users 0 members are here
  • project
  • matrix
  • esp8266
  • printing
  • arduino
Related

Need Hardware list for 5-Dot-Matrix printing with Wifi-Modules

capt_kaplan
capt_kaplan over 8 years ago

Hello guys
I just received a project from my local Soccer-Club to be able to print letters on the play field (grass-surface).
Mainly for cheering purposes, maybe also for advertisement later on.
The idea is pretty straight forward:

There are 5 RC-Cars with down facing spray cans, used as printers [-P-] as shown below.

Those 5 RC-Cars have all the same specs, this means you can expect one defined speed V.

 

   O O O       O O O          O O O       O    -P-|RC-Car-1

O              O          O    O           O    O    -P-|RC-Car-2

O              O          O    O           O    O    -P-|RC-Car-3

O              O          O    O           O    O    -P-|RC-Car-4

   O O O       O O O          O O O       O O -P-|RC-Car-5

              ----->V

(I hope it is obvious that this is going to write "COOL" ^^)

 

All those "O" 's represent a spray-puff and thus generating letters with this so called 5-Dot-Matrix method.
The challenge is to make it wireless (WiFi).
I was thinking of getting:
5* ESP8266 v-07 ( I choose v-07 to be able to add an antenna if increased range is needed in the future)

1* Arduino Uno, this one will be carry the code for the pre-selected words. (This can also be carried by RC-Car-3 as so called Leader/Commander)

5* Servos to interact with the spray cans to create those puffs

5* 3.3V Power supplies (Maybe Coin-Cell battery) for the ESP8266's

1* Battery for the Arduino Uno
But I am not sure if i can even work with this setup.

 

I mean I need to be able to connect everything like this (unless someone tells me otherwise):

 

Spray-can - Servo - ESP8266 = RC-Car-1

Spray-can - Servo - ESP8266 = RC-Car-2

Spray-can - Servo - ESP8266 - Arduino Uno = RC-Car-3

Spray-can - Servo - ESP8266 = RC-Car-4

Spray-can - Servo - ESP8266 = RC-Car-5

 

As mentioned the Arduino Uno contains the commands for all the other RC-Cars. This means that ESP8266 connected to that Arduino needs to be able to independently control (over WiFi) 5 Servos.
Servo from RC-Car-1 & RC-Car-2 & RC-Car-4 & RC-Car-5 & its own servo. Is it even possible to connect one ESP8266 with 4 other ESP8266 over WiFi at the same time? Does it even have to be at the same time? I could perhaps add delays (sleep-times) with experimenting...
Is there already a code for 5 Dot-Matix Printing?

 

 

 

 

 

 

 

 

 

Thank you very much for your attention

 

Best regards.

 

Capt_Kaplan

 

 

 

 

 

P.S. : It has to be over WiFi with 5 independent RC-Cars. I know it could make my project way easier if i just added a long stick of PVC-Pipe and made wired connections to each Servo and mount that on rails or something, but this needs to be versatile.