Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Program an Arduino with another Arduino
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 7 answers
  • Subscribers 421 subscribers
  • Views 2763 views
  • Users 0 members are here
  • arduino
  • programmer
Related

Program an Arduino with another Arduino

rishi2628
rishi2628 over 9 years ago

image

 

Is there any way I can program an Arduino using another Arduino,without the need of any computer. I want to store the programming code in the EEPROM of the "Programmer Arduino" and using any interface like SPI, I2C or Serial, burn this code to the Second arduino. Is it possible and how can it be implemented ?

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 9 years ago in reply to clem57 +2 suggested
    clem57 That link is for programming the bootloader into a blank 328 chip. If I read the OP right, he wants to use an Arduino to replace the program contents. I'm sure there is a method of poking data onto…
  • rishi2628
    rishi2628 over 9 years ago +1 suggested
    Actually I was looking for a solution something like this :- https://www.youtube.com/watch?v=M-sFQNIXde8
Parents
  • clem57
    0 clem57 over 9 years ago

    Here is a way How to program a AVR (arduino) with another arduino

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mcb1
    0 mcb1 over 9 years ago in reply to clem57

    clem57 That link is for programming the bootloader into a blank 328 chip.

     

     

    If I read the OP right, he wants to use an Arduino to replace the program contents.

    I'm sure there is a method of poking data onto the ram parts of an Arduino, but it's certainly beyond me.

     

    One thing I can offer is that the EEPROM doesn't have enough room to store that amount of data.

     

    rishi2628 is more than capable of using Google ....  just as I would .... image

     

     

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • mcb1
    0 mcb1 over 9 years ago in reply to clem57

    clem57 That link is for programming the bootloader into a blank 328 chip.

     

     

    If I read the OP right, he wants to use an Arduino to replace the program contents.

    I'm sure there is a method of poking data onto the ram parts of an Arduino, but it's certainly beyond me.

     

    One thing I can offer is that the EEPROM doesn't have enough room to store that amount of data.

     

    rishi2628 is more than capable of using Google ....  just as I would .... image

     

     

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • beacon_dave
    0 beacon_dave over 9 years ago in reply to mcb1

    Something more like uProg perhaps ?

    https://www.youtube.com/watch?v=tg67HWwBRlY

    µProg – tiny, fast, portable AVR programmer with SD – mdiy.pl

     

    Another interesting looking project is Phoenard which appears to be able to store and then recall multiple Arduino sketches without the laptop/IDE.

    https://www.youtube.com/watch?v=bAFTAbY9mdk

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 9 years ago in reply to mcb1

    Clem you are right! By a certain point of view it is the way to program the bootloader and I have already done this in past in a lot of cases. I have used a UNO instead of a Mega but there are just the pins connection differences.

    This is also the way - not yet personally tested - to program directly a chip without the bootloader. I read something about in past but I was no longer able to find the link. Is a lack of my memory or this is a reasonable option?

     

    Enrico