Arduino
  • Products
  • More
Arduino
Arduino Forum How do I figure out the orientation of a accellerometer?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 417 subscribers
  • Views 1138 views
  • Users 0 members are here
  • mpu-6050
  • accellerometer
  • arduino
Related

How do I figure out the orientation of a accellerometer?

kthomsen
kthomsen over 9 years ago

Hi,

 

I am trying to make my own "TrakDot" luggage tracking device, and for that I am gonna make the feature that disables all the antennas when the airplane leaves the ground (accelerates) and when it lands again (decelerates).

But since I don't have a lot of experience with accellerometers, I can't really figure out how to approach the following:

 

How can I figure out what orientation the accellerometer is in? I mean, if I put it in my suitcase, it could be pointing north, south, east, west, 45* angle or be upside down after the baggage-guys have thrown it around a few times.. How do I know/register that the airplane accelerates when I don't know if it's accelerating on X or Y or somewhere in between?

 

I am using the  MPU-6050MPU-6050 module which also has an integrated gyroscope maybe somehow that can help me determine on what axis I should measure the acceleration

 

Thanks!

-Kenneth

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 9 years ago +1 suggested
    Interesting problem. The only constant acceleration is gravity, all other accelerations are transient, so when the acceleration doesn't change for long periods of time it means the bag is stationary or…
Parents
  • michaelkellett
    0 michaelkellett over 9 years ago

    It's no at all easy to work out when a plane leaves the ground or lands just by acceleration. You could probably detect the take off by looking at acceleration along the ground but it would be very easy to get false triggers for landing.

     

    You would need to record lots of flight data and then devise a way of processing the data to correctly identify what was happening. Adding a pressure sensor might help (if it's in the hold).

     

    It is easy to work out the orientation of a DC coupled accelerator if it isn't being accelerated (it might be hard to know this)  - but you can vector sum the readings from the XYZ axes and this (when the accelerometer is at constant velocity) will give you the angle of the earth's 1g gravity relative to the accelerometer.

     

    The accelerometers and gyros in  MPU-6050MPU-6050 are not good enough to do classical inertial guidance but they can work in sensor fusion type applications to give useful information InvenSense may have some applications data that will help otherwise expect to do a lot of Googling and reading

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • kthomsen
    0 kthomsen over 9 years ago in reply to michaelkellett

    Thank you Michael!

     

    I had an idea that this wasn't gonna be an easy task, and I also had the idea that it would take a lot of research and flight data.

    I travel often, so hopefully I could make a tiny "beta" device that would track and log the data on and SD card, but for that, I would need to know how to get the correct data in the first place! image

     

    So I will try and look into what you wrote, and see if I can figure something out to do this for me! image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • kthomsen
    0 kthomsen over 9 years ago in reply to michaelkellett

    Thank you Michael!

     

    I had an idea that this wasn't gonna be an easy task, and I also had the idea that it would take a lot of research and flight data.

    I travel often, so hopefully I could make a tiny "beta" device that would track and log the data on and SD card, but for that, I would need to know how to get the correct data in the first place! image

     

    So I will try and look into what you wrote, and see if I can figure something out to do this for me! image