Arduino Forum Reading 0 to 100mV On Arduino Uno
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
  • State Verified Answer
  • Replies 5 replies
  • Answers 1 answer
  • Subscribers 402 subscribers
  • Views 2385 views
  • Users 0 members are here
Related

Reading 0 to 100mV On Arduino Uno

gregn67
gregn67 over 8 years ago

I have a project that I need some help with...

 

We have a signal that ranges from 0 to about 100mV.  We need to translate that to a tone that gets louder as the voltage goes up.

 

I have an Arduino Uno board and have written a quick Scratch program (using ScratchX) that reads A0 and set's the volume of a tone based on that value.

 

But, I think that this will only work for 0 to 5V signals.

 

Is there a way to increase the sensitivity of the analog inputs?

 

Thanks in advance!!

 

Greg

  • Sign in to reply
  • Cancel

Top Replies

  • rachaelp
    rachaelp over 8 years ago in reply to gregn67 +3 verified
    The ADC on the Arduino is either 10-bit or 12-bit depending on the model. That means that your read value is in integer between 0 and 1023 for the 10-bit ones and 0 and 4095 for the 12-bit ones. So you…
  • rachaelp
    rachaelp over 8 years ago +2 suggested
    Hi Greg, The map() function should scale the input range for you. See here: https://www.arduino.cc/en/Reference/Map Bear in mind that with a 0-100mV signal you'll have limited resolution and your steps…
  • gregn67
    gregn67 over 8 years ago in reply to rachaelp +2
    It's all starting to make sense to me now!! The map function works perfectly!! Thanks soooo much!! Greg
  • rachaelp
    0 rachaelp over 8 years ago

    Hi Greg,

     

    The map() function should scale the input range for you. See here: https://www.arduino.cc/en/Reference/Map

     

    Bear in mind that with a 0-100mV signal you'll have limited resolution and your steps will be large. A better solution is to scale the signal with an amplifier external to the Arduino so that it becomes a 0-5V signal into the ADC to make the best of the resolution of the ADC.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • gregn67
    0 gregn67 over 8 years ago in reply to rachaelp

    So... to make sure I understand this correctly...

     

    If I wanted to change the analog pin 0 from 0 to 5V to 0 to 0.5V, I would use this command;

         map(0, 0, 5, 0, 0.5);

     

    Thanks for suggestion...

     

    Greg

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 8 years ago in reply to gregn67

    The ADC on the Arduino is either 10-bit or 12-bit depending on the model. That means that your read value is in integer between 0 and 1023 for the 10-bit ones and 0 and 4095 for the 12-bit ones. So you can look at what range your are seeing from the read of the ADC and scale it to a range which works for what you are doing. So depending on what you are doing in your code it might just be a case of using an appropriate range for the values you are reading or you can use map() to make them more convenient for what you are doing.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • gregn67
    0 gregn67 over 8 years ago in reply to rachaelp

    It's all starting to make sense to me now!!

     

    The map function works perfectly!!

     

    Thanks soooo much!!

     

    Greg

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 8 years ago in reply to gregn67

    You're welcome. Glad to hear it's all working for you now image