Arduino
  • Products
  • More
Arduino
Arduino Forum EASY -> Arduino Robot (line following / rescue) gone wrong :(
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 6 answers
  • Subscribers 403 subscribers
  • Views 932 views
  • Users 0 members are here
  • arduino 101
  • arduino-robot
  • robotics
  • help!!
  • education help
  • robot kit
  • help!
Related

EASY -> Arduino Robot (line following / rescue) gone wrong :(

the_future
the_future over 8 years ago

Hey guys!

 

Need help! I get this message "Low memory available, stability problems may occur."

then the robot will search for a line but then struggles to follow the path.

 

 

 

CODE from example:

 

/* Robot Rescue

 

 

In this example, the robot enters the line following mode and

plays some music until it reaches its target. Once it finds the

target, it pushes it out of the track. It then returns to the

track and looks for a second target.

 

 

You can make the robot push as many objects as you want to, just

add more to calls to the rescue function or even move that code

into the loop.

 

 

Circuit:

* Arduino Robot

* some objects for the robot to push

* a line-following circuit

 

 

created 1 May 2013

by X. Yang

modified 12 May 2013

by D. Cuartielles

 

 

This example is in the public domain

*/

 

 

#include <ArduinoRobot.h> // include the robot library

#include <Wire.h>

#include <SPI.h>

 

 

void setup() {

  // initialize the Robot, SD card, display, and speaker

  Robot.begin();

  Robot.beginTFT();

  Robot.beginSD();

  Robot.beginSpeaker();

 

 

  // draw "lg0.bmp" and "lg1.bmp" on the screen

  Robot.displayLogos();

 

 

  // display the line following instructional image from the SD card

  Robot.drawBMP("lf.bmp", 0, 0);

 

 

  // play the chase music file

  Robot.playFile("chase.sqm");

 

 

  // add the instructions

  Robot.text("Rescue\n\n place the robot on\n the rescue track\n pushing the\n obstacles away", 5, 5);

  Robot.text("Press the middle\n button to start...", 5, 61);

  Robot.waitContinue();

 

 

  // start

  Robot.fill(255, 255, 255);

  Robot.stroke(255, 255, 255);

  Robot.rect(0, 0, 128, 80); // erase the previous text

  Robot.stroke(0, 0, 0);

  Robot.text("Start", 5, 5);

 

 

  // use this to calibrate the line following algorithm

  // uncomment one or the other to see the different behaviors of the robot

  // Robot.lineFollowConfig(14, 9, 50, 10);

  Robot.lineFollowConfig(11, 7, 60, 5);

 

 

  // run the rescue sequence

  rescueSequence();

  // find the track again

  goToNext();

  // run the rescue sequence a second time

  rescueSequence();

 

  // here you could go on ...

 

 

}

 

 

void loop() {

  //nothing here, the program only runs once.

}

 

 

// run the sequence

void rescueSequence() {

  //set the motor board into line-follow mode

  Robot.setMode(MODE_LINE_FOLLOW);

 

 

  while (!Robot.isActionDone()) { // wait until it is no longer following the line

  }

  delay(1000);

 

 

  // do the rescue operation

  doRescue();

  delay(1000);

}

 

 

void doRescue() {

  // Reached the endline, engage the target

  Robot.motorsWrite(200, 200);

  delay(250);

  Robot.motorsStop();

  delay(1000);

 

 

  // Turn the robot

  Robot.turn(90);

  Robot.motorsStop();

  delay(1000);

 

 

  // Move forward

  Robot.motorsWrite(200, 200);

  delay(500);

  Robot.motorsStop();

  delay(1000);

 

 

  // move backwards, leave the target

  Robot.motorsWrite(-200, -200);

  delay(500);

  Robot.motorsStop();

}

 

 

void goToNext() {

  // Turn the robot

  Robot.turn(-90);

  Robot.motorsStop();

  delay(1000);

}

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 8 years ago +1 suggested
    I assume your using an Arduino UNO for this or at least an ATMEGA328 based controller It is a classic memory hog when you add SD card libraries and the like, you also have sound and graphics on the go…
  • Robert Peter Oakes
    Robert Peter Oakes over 8 years ago in reply to Robert Peter Oakes +1 suggested
    so remove things like Robot.beginSD(); Robot.beginSpeaker(); and the graphics cosmetics like // draw "lg0.bmp" and "lg1.bmp" on the screen Robot.displayLogos(); // display the line following instructional…
  • Robert Peter Oakes
    Robert Peter Oakes over 8 years ago in reply to Robert Peter Oakes +1 suggested
    I missed one, also remove this // play the chase music file Robot.playFile("chase.sqm");
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 8 years ago

    I assume your using an Arduino UNO for this or at least an ATMEGA328 based controller

     

    It is a classic memory hog when you add SD card libraries and the like, you also have sound and graphics on the go. there are a few things you can do to claw back dome memory

     

    1. reduce the size of those text strings (Even temporary to test)

    2. remove the speaker stuff (Again to test)

    3. there may be some things in the library you can also shrink (Buffers are used all over what you have there) and they all take up ram.

    4. if you have one, try and run on an ATMEGA (Arduino MEGA2560)

     

    The one issue with the Arduino Sketches is that if you run out of memory, the ONLY indication you get is the program behaving unexpectedly or crashing altogether. you won't get a trappable error to tell you it failed, it will just start over writing areas of RAM, executing weird parts of code etc. the only way to be sure is to remove bits of code that are not essential to the basic functionality of the project.

     

    the biggest hog you probably have is the SD Card libraries, try find a "LITE" version perhaps or see if there are options to reduce the buffers it uses.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 8 years ago in reply to Robert Peter Oakes

    so remove things like

    Robot.beginSD();

    Robot.beginSpeaker();

     

    and the graphics cosmetics like

    // draw "lg0.bmp" and "lg1.bmp" on the screen

      Robot.displayLogos();

    // display the line following instructional image from the SD card

      Robot.drawBMP("lf.bmp", 0, 0);

     

    these dont seem to be essential to the main function of the bot and may be enough to remove the compiler warnings and allow the code to work correctly

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 8 years ago in reply to Robert Peter Oakes

    so remove things like

    Robot.beginSD();

    Robot.beginSpeaker();

     

    and the graphics cosmetics like

    // draw "lg0.bmp" and "lg1.bmp" on the screen

      Robot.displayLogos();

    // display the line following instructional image from the SD card

      Robot.drawBMP("lf.bmp", 0, 0);

     

    these dont seem to be essential to the main function of the bot and may be enough to remove the compiler warnings and allow the code to work correctly

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • Robert Peter Oakes
    0 Robert Peter Oakes over 8 years ago in reply to Robert Peter Oakes

    I missed one, also remove this

      // play the chase music file

      Robot.playFile("chase.sqm");

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
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
An Avnet Company © 2025 Premier Farnell Limited. All Rights Reserved.