Arduino Forum EASY -> Arduino Robot (line following / rescue) problem pt2
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
  • State Suggested Answer
  • Replies 1 reply
  • Answers 1 answer
  • Subscribers 391 subscribers
  • Views 267 views
  • Users 0 members are here
  • noobs
  • help!!
  • education help
  • noob
  • arduino_robot
  • urgent
  • robot kit
  • help!
  • arduino
Related

EASY -> Arduino Robot (line following / rescue) problem pt2

the_future
the_future over 8 years ago

Hey Guys!

 

Got rid of the "low memory" problem thanks to a friend on my last question

 

THE PROBLEM NOW IS -> after searching for the black line The Arduino Robot struggles to move forward and the display flickers.

                                            Never gets to the part where it saves the object image

 

 

MEANT TO BE LIKE THIS -> https://www.youtube.com/watch?v=bnqDzNAU7JQ&t=584s

 

 

CODE

 

 

#include <ArduinoRobot.h> // include the robot library

#include <Wire.h>

#include <SPI.h>

 

 

void setup() {

  Robot.begin();

  Robot.beginTFT();

 

 

  // add the instructions

  Robot.text("Rescue\n\n place the robot on\n the rescue track\n pushing the\n obstacles away", 5, 5);

  Robot.text("Press the middle\n button to start...", 5, 61);

  Robot.waitContinue();

 

 

  // start

  Robot.fill(255, 255, 255);

  Robot.stroke(255, 255, 255);

  Robot.rect(0, 0, 128, 80); // erase the previous text

  Robot.stroke(0, 0, 0);

  Robot.text("Start", 5, 5);

 

 

  // use this to calibrate the line following algorithm

  // uncomment one or the other to see the different behaviors of the robot

  // Robot.lineFollowConfig(14, 9, 50, 10);

  Robot.lineFollowConfig(11, 7, 60, 5);

 

 

  // run the rescue sequence

  rescueSequence();

  // find the track again

  goToNext();

  // run the rescue sequence a second time

  rescueSequence();

}

 

 

void loop() {

  //nothing here, the program only runs once.

}

 

 

// run the sequence

void rescueSequence() {

  //set the motor board into line-follow mode

  Robot.setMode(MODE_LINE_FOLLOW);

 

 

  while (!Robot.isActionDone()) { // wait until it is no longer following the line

  }

  delay(1000);

 

 

  // do the rescue operation

  doRescue();

  delay(1000);

}

 

 

void doRescue() {

  // Reached the endline, engage the target

  Robot.motorsWrite(200, 200);

  delay(250);

  Robot.motorsStop();

  delay(1000);

 

 

  // Turn the robot

  Robot.turn(90);

  Robot.motorsStop();

  delay(1000);

 

 

  // Move forward

  Robot.motorsWrite(200, 200);

  delay(500);

  Robot.motorsStop();

  delay(1000);

 

 

  // move backwards, leave the target

  Robot.motorsWrite(-200, -200);

  delay(500);

  Robot.motorsStop();

}

 

 

void goToNext() {

  // Turn the robot

  Robot.turn(-90);

  Robot.motorsStop();

  delay(1000);

}

  • Sign in to reply
  • Cancel

Top Replies

  • clem57
    clem57 over 8 years ago +1 suggested
    See EASY -> Arduino Robot (line following / rescue) gone wrong for current discussions. Why open a new blog?
Parents
  • clem57
    0 clem57 over 8 years ago

    See EASY -> Arduino Robot (line following / rescue) gone wrong image  for current discussions. Why open a new blog?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 8 years ago

    See EASY -> Arduino Robot (line following / rescue) gone wrong image  for current discussions. Why open a new blog?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer