Arduino Forum New guy here with question -
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
  • State Suggested Answer
  • Replies 6 replies
  • Answers 6 answers
  • Subscribers 403 subscribers
  • Views 624 views
  • Users 0 members are here
Related

New guy here with question -

nealbopper
nealbopper over 8 years ago

Hello, New member here. I am new to the Arduino and programming but I want to take on a project that includes my Chicken Coop. I have an inclosed Chicken Coop and a Chicken run, The coop has a small run inside of it but it's not large enough for 9 Chickens for a full day so I am wanting to create 2 auromatic doors but I need to ask a question. is it possible to run 2 separate motors that will not be running at the same time. Once door will open the interior coop door and the other motor will open the coop door to the chicken run so my chickens can roam. I have a 60w solar panel, controller and 12v marine battery. I have the arduino Uno, motor controller, Arduino clock and limit switches with a breadboard. The motor I want to use is a 12v DeWalt drill motor. If it's possible to run 2 separate motors, I will pick up the neccessary hardware and motor for the 2nd operation. Please let me know what you think. Thank you in advance.

  • Sign in to reply
  • Cancel

Top Replies

  • rachaelp
    rachaelp over 8 years ago +1 suggested
    Hi Neal, Welcome to the Element 14 forums, you should find it a very friendly place generally with lots of experienced people willing to help out I have a couple of questions, firstly what motor controller…
  • nealbopper
    nealbopper over 8 years ago in reply to rachaelp +1 suggested
    Hello Rachael, I am at work right now but I will get the DeWalt 12v drill motor and look the specs up. The motor Controller is the typical Arduino controller: Qunqi L298N Motor Drive Controller Board Module…
  • rachaelp
    rachaelp over 8 years ago in reply to nealbopper +1 suggested
    Hi Neal, Ok no problem, let us know what you find out about the motor. I think I found a link to the manual for a similar motor driver to the one you mention and it looks like it'll do two DC motors okay…
Parents
  • DAB
    0 DAB over 8 years ago

    Hi Neal,

     

    You can test out your logic by first attaching LED's to your Arduino outputs.

     

    Basically, if you can get the LED's to light in the proper sequence, then you can control the motors just as easily.

     

    Then you can try the motors one at a time to make sure you have the correct timing and you can assess current draw.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • DAB
    0 DAB over 8 years ago

    Hi Neal,

     

    You can test out your logic by first attaching LED's to your Arduino outputs.

     

    Basically, if you can get the LED's to light in the proper sequence, then you can control the motors just as easily.

     

    Then you can try the motors one at a time to make sure you have the correct timing and you can assess current draw.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer