Arduino Forum Hooking Arduino Uno into Solar power?
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
  • State Verified Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 402 subscribers
  • Views 483 views
  • Users 0 members are here
Related

Hooking Arduino Uno into Solar power?

nealbopper
nealbopper over 8 years ago

Hello again,

I looked for this topic and am surprised there isn't a million topics on this but here's my question. I have a 60w solar panel, a solar regulator and a 12v marine battery for my Chicken coop project.

I want to hook my Arduino Uno automatic door opener to this system but am hesitant to hook it up in fear of burning the system up. Is there a product I need to look into that will regulate the power coming

into the Arduino and my motor controller? They are separate power sources and I would think I need to treat them differently. An in line fuse perhaps? Any suggestions?

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 8 years ago +4 suggested
    Hi Neal, The voltage will determine how much current a given device takes not how much the source can potentially deliver. Your source may be able to deliver a lot of power at 12 volts but the UNO will…
  • jw0752
    jw0752 over 8 years ago in reply to nealbopper +2 verified
    Hi Neal, Here is a link to the Data Sheet so you can see how a typical circuit would be set up. The data sheet covers all the different voltage versions of this chip but you will be interested in the 5…
  • jw0752
    0 jw0752 over 8 years ago

    Hi Neal,

    The voltage will determine how much current a given device takes not how much the source can potentially deliver. Your source may be able to deliver a lot of power at 12 volts but the UNO will take the same amount of power regardless of whether it is hooked to a 12 volt small power source or a 12 volt large power source. The UNO has an internal voltage regulator that takes the voltage delivered to the power jack or the Vin pin and reduces it to 5 volts for the use of the circuitry. 12 volts is on the upper edge of what the internal regulator can handle and a Vin voltage of 9 volts is more common. To be safe you could use a 7805 regulator IC and feed its output to the 5V power pin of the UNO.

    John

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • nealbopper
    0 nealbopper over 8 years ago in reply to jw0752

    Thanks for the advice John, I will look that product up now. Thanks for the prompt response sir.image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 8 years ago in reply to nealbopper

    Hi Neal,

     

    Here is a link to the Data Sheet so you can see how a typical circuit would be set up. The data sheet covers all the different voltage versions of this chip but you will be interested in the 5 volt version the 7805.

     

    http://www.farnell.com/datasheets/2196360.pdf?_ga=1.127026893.118307707.1475274175

     

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer