Arduino Forum Arduino
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
  • State Suggested Answer
  • Replies 8 replies
  • Answers 3 answers
  • Subscribers 407 subscribers
  • Views 864 views
  • Users 0 members are here
  • frontpage
Related

Arduino

kushali
kushali over 8 years ago

I would like to get an arduino code for the following requirements

The system should monitor the temperature of the room.

 Light different LEDs depending on the temperature

 Sound an alarm if it is too hot.

 Activate a fan through a transistor to cool the system down if it gets above a certain temperature.

 Use different fan speeds depending on the temperature by pulsing the fan.

 Implement an alarm reset system using a code sequence from button presses.

 It should only work when the lights are on, using an LDR.

 Use a potentiometer as a calibration mechanism.

 Print out an array of information on request of a button press, including temperature in K, C, F, and system state.

 Allow all aspects of the system to be configured using variables.

  • Sign in to reply
  • Cancel

Top Replies

  • balearicdynamics
    balearicdynamics over 8 years ago in reply to clem57 +6
    Sounds like another final exam task
  • mcb1
    mcb1 over 8 years ago in reply to balearicdynamics +6 suggested
    looks that way
  • clem57
    clem57 over 8 years ago +2 suggested
    Show me the wiring of the hardware with a Fritz model and I can get you started.
Parents
  • rsc
    0 rsc over 8 years ago

    There are hundreds of examples with code on the web:

    https://www.arduino.cc/en/Tutorial/BuiltInExamples

    Make Your Own Temperature Controller with an Arduino

    Arduino Temperature Controlled Relay - Tutorial #6

    Arduino Fan Speed Controlled by Temperature

    Home Automation: Fan Control with Arduino

    Temperature Control With Arduino and PWM Fans

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • rsc
    0 rsc over 8 years ago

    There are hundreds of examples with code on the web:

    https://www.arduino.cc/en/Tutorial/BuiltInExamples

    Make Your Own Temperature Controller with an Arduino

    Arduino Temperature Controlled Relay - Tutorial #6

    Arduino Fan Speed Controlled by Temperature

    Home Automation: Fan Control with Arduino

    Temperature Control With Arduino and PWM Fans

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer