Arduino Forum Chain RGB LED - Arduino
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
  • State Not Answered
  • Replies 5 replies
  • Subscribers 393 subscribers
  • Views 557 views
  • Users 0 members are here
  • rgb led chain
Related

Chain RGB LED - Arduino

faiznur4h61
faiznur4h61 over 8 years ago

I would like to chain up 64x32 RGB matrix LED by using Arduino. Is there any way to make it?

  • Sign in to reply
  • Cancel

Top Replies

  • beacon_dave
    beacon_dave over 8 years ago +1
    Perhaps look at using a HypnoCube HypnoLSD serial driver between the Aduino and the LED matrix hypnocube | Hypnocube LED Serial Driver https://www.youtube.com/watch?v=SzpcPrnh9LY Single HypnoLSD serial…
Parents
  • koudelad
    0 koudelad over 8 years ago

    Is it something you want to use for your hobby or something to be produced commercially?

     

    64 x 32 x 3 colors equals to 6144 channels to be driven.

    I wouldn't personally want to build that myself from port expanders like PCF8575.

     

    How about using some ready-made module like this one? Have a look at the display datasheet there with a photo of that module from the rear, with all the ICs.

    I think they already did some calculations to support this statement "Please note you cannot use an Arduino UNO to drive this size, its way too big! Use an Arduino Mega, Raspberry Pi, BBB or other device that can handle displaying to RGB matricies and has plenty of RAM."

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • faiznur4h61
    0 faiznur4h61 over 8 years ago in reply to koudelad

    Hi there.. This is something that I have to study under R&D.. I get the 64x32 LED panel for 12 units. Yes, it just like this one but to make it chain to each other and build up until 4x3 panel of 64x32 is hard to do. Now I am using arduino Mega ADK with the library given by gitHub. unfortunately, the library only support to display 1 panel of 64x32 RGB LED only.. image

    Now I am stuck and have no idea how to make it. Still trying to adjust the library and produce the compatible one with chain panel application.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • faiznur4h61
    0 faiznur4h61 over 8 years ago in reply to koudelad

    Hi there.. This is something that I have to study under R&D.. I get the 64x32 LED panel for 12 units. Yes, it just like this one but to make it chain to each other and build up until 4x3 panel of 64x32 is hard to do. Now I am using arduino Mega ADK with the library given by gitHub. unfortunately, the library only support to display 1 panel of 64x32 RGB LED only.. image

    Now I am stuck and have no idea how to make it. Still trying to adjust the library and produce the compatible one with chain panel application.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • the-dubster
    0 the-dubster over 8 years ago in reply to faiznur4h61

    If you can drive one panel then can you multiplex them?

     

    Use the same code to drive each in sequence, it's the way multiple 7 segment  displays can be driven using 7 outputs + 1 for each individual digit to enable them.