Arduino Forum How to detect usage of height adjustable table?
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
  • State Suggested Answer
  • Replies 12 replies
  • Answers 7 answers
  • Subscribers 394 subscribers
  • Views 1475 views
  • Users 0 members are here
  • barometric sensor
  • motion detecting
  • accelerometer
  • proximity sensors
Related

How to detect usage of height adjustable table?

svendsen2032
svendsen2032 over 8 years ago

Hi at element14

 

 

We have been trying to solve this matter for quite some time now, and we simply haven't been able to come up with a satisfying solution. We are working on a little "bot" placed on top of a height adjustable desk. The bot has to measure whether the desk is in a sitting or standing position. So we do either need to measure the movement and direction of movement or the height of the table. We have had some luck using proximity sensors (IR and US), but they are very dependent on the environment and placement, as e.g. a desk lamp can make the readings worthless.

 

 

We are now working with an accelerometer and/or a barometric sensor, but the acceleration of a table is very small and the height difference of the table is only 20-40 cm's. So the sensors have to be very precise and sensitive.

 

 

Soo, do you maybe have other ideas to what sensors we could use? Or maybe some insights into how we can get the accelerometer and barometric sensors to work properly? - would be a of great help image

 

Best regards Mads

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 8 years ago in reply to svendsen2032 +2 suggested
    So we are trying to register everytime the users changes working position from sitting to standing and from standing to sitting You could use an ultrasonic sensor and detect the height to the ceiling.…
  • DAB
    DAB over 8 years ago +1 suggested
    Hi Mads, Have you considered using a capacitive sensor mounted to the desk? The TI sensor system can accurately detect objects up to about 50 cms. Another way would be to use a light and a camera to measure…
  • vandia
    vandia over 8 years ago +1 suggested
    On the note of what you're trying to do, you've giving detail of your method, but it still leaves your end goal rather vague.... especially with "acceleration of a table". It leaves the questions: "Is…
Parents
  • koudelad
    0 koudelad over 8 years ago

    Hello,

    is the table height adjusted by some electronic control or a manual handle?

     

    I use two types of these tables (both electronically controlled) and the manufacturer offers them with two types of controllers. The first one has only up and down keys, the second one has up and down keys, 7 segment display to display the height in centimetres and four keys to store / restore value from a memory. These controllers are interchangeable which means there is probably a rotary encoder on the motor shaft and only one of these controllers can make use of the output image The controller of course has then no idea about the ground clearance etc., it just knows the relative position to the lowest position. (Note: I haven't personally dismantled the mechanism.) I would try to do my own version of the controller in this case.

     

    If you wanted to attach the measurement sensor to all kinds of mechanical tables (parallel with the floor), an ultrasonic sensor is one of the options. You don't even need to measure the absolute ground clearance, just the difference between the positions.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • koudelad
    0 koudelad over 8 years ago

    Hello,

    is the table height adjusted by some electronic control or a manual handle?

     

    I use two types of these tables (both electronically controlled) and the manufacturer offers them with two types of controllers. The first one has only up and down keys, the second one has up and down keys, 7 segment display to display the height in centimetres and four keys to store / restore value from a memory. These controllers are interchangeable which means there is probably a rotary encoder on the motor shaft and only one of these controllers can make use of the output image The controller of course has then no idea about the ground clearance etc., it just knows the relative position to the lowest position. (Note: I haven't personally dismantled the mechanism.) I would try to do my own version of the controller in this case.

     

    If you wanted to attach the measurement sensor to all kinds of mechanical tables (parallel with the floor), an ultrasonic sensor is one of the options. You don't even need to measure the absolute ground clearance, just the difference between the positions.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer