Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum How to detect usage of height adjustable table?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 12 replies
  • Answers 7 answers
  • Subscribers 418 subscribers
  • Views 2263 views
  • Users 0 members are here
  • barometric sensor
  • motion detecting
  • accelerometer
  • proximity sensors
Related

How to detect usage of height adjustable table?

svendsen2032
svendsen2032 over 9 years ago

Hi at element14

 

 

We have been trying to solve this matter for quite some time now, and we simply haven't been able to come up with a satisfying solution. We are working on a little "bot" placed on top of a height adjustable desk. The bot has to measure whether the desk is in a sitting or standing position. So we do either need to measure the movement and direction of movement or the height of the table. We have had some luck using proximity sensors (IR and US), but they are very dependent on the environment and placement, as e.g. a desk lamp can make the readings worthless.

 

 

We are now working with an accelerometer and/or a barometric sensor, but the acceleration of a table is very small and the height difference of the table is only 20-40 cm's. So the sensors have to be very precise and sensitive.

 

 

Soo, do you maybe have other ideas to what sensors we could use? Or maybe some insights into how we can get the accelerometer and barometric sensors to work properly? - would be a of great help image

 

Best regards Mads

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 9 years ago in reply to svendsen2032 +2 suggested
    So we are trying to register everytime the users changes working position from sitting to standing and from standing to sitting You could use an ultrasonic sensor and detect the height to the ceiling.…
  • DAB
    DAB over 9 years ago +1 suggested
    Hi Mads, Have you considered using a capacitive sensor mounted to the desk? The TI sensor system can accurately detect objects up to about 50 cms. Another way would be to use a light and a camera to measure…
  • vandia
    vandia over 9 years ago +1 suggested
    On the note of what you're trying to do, you've giving detail of your method, but it still leaves your end goal rather vague.... especially with "acceleration of a table". It leaves the questions: "Is…
Parents
  • DAB
    0 DAB over 9 years ago

    Hi Mads,

     

    Have you considered using a capacitive sensor mounted to the desk?

     

    The TI sensor system can accurately detect objects up to about 50 cms.

     

    Another way would be to use a light and a camera to measure spot size, but now you are adding some complexity.

     

    Maybe an ultrasonic sensor?

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • svendsen2032
    0 svendsen2032 over 9 years ago in reply to DAB

    I'm not sure I do fully understand. Do you suggest to use a capacitive sensor to measure the electrical field of the motors? Or, how do you figure it's possible to detect movement with a capicitive sensor?

     

    And a camera might be a bit too complex and we do experience users linking cameras to surveillance, which ain't good.

     

    We have been using ultrasonic sensors and they do work, however they are very dependent on the environment.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • DAB
    0 DAB over 9 years ago in reply to svendsen2032

    Should be easy.

    Just lay down a conductive strip near the keyboard and connect it to the capacitive sensing circuit.

    When the compute keyboard is on the desk, you get a good reading when the hands are on the keyboard.

    If the keyboard is raised to a standing position, then the reading will be less and can probably provide you with a fairly precise distance from the desk top.

     

    A simple program can check the height every time the computer is in use, so you can record trend data over time.

     

    Clean, simple and automatic.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • DAB
    0 DAB over 9 years ago in reply to svendsen2032

    Should be easy.

    Just lay down a conductive strip near the keyboard and connect it to the capacitive sensing circuit.

    When the compute keyboard is on the desk, you get a good reading when the hands are on the keyboard.

    If the keyboard is raised to a standing position, then the reading will be less and can probably provide you with a fairly precise distance from the desk top.

     

    A simple program can check the height every time the computer is in use, so you can record trend data over time.

     

    Clean, simple and automatic.

     

    DAB