Arduino Forum Using 40 low frequency Mics.
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
  • State Suggested Answer
  • Replies 21 replies
  • Answers 12 answers
  • Subscribers 394 subscribers
  • Views 2653 views
  • Users 0 members are here
Related

Using 40 low frequency Mics.

noblemaster
noblemaster over 8 years ago

Hi,

I am working on a device that takes input from 40 microphones and send data to PC via Arduino.

I want to use low frequency microphones (5Hz onwards) with around 200-250Hz sampling for each mic.

 

For this purpose, my preliminary design is like this...

    40 Mics --> 40 PreAmp circuits --> Mux Shield II --> Arduino DUE --> PC

 

Please suggest me suitable commercial available preAmp circuits and any suggestion on the design is most welcome.

 

Thanks.

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 8 years ago in reply to noblemaster +2 suggested
    Your answer suggests you are willing to spend over $1000 per channel to get the best possible. If that is not true, the description needs to be more complete in order to get a helpful answer.
  • michaelkellett
    michaelkellett over 8 years ago in reply to noblemaster +2 suggested
    To measure at up to 100Hz you need to sample each microphone at 500Hz or faster. For each microphone you will need a a buffer amplifier as shown on the Invensys data sheet and an anti-aliasing low pass…
  • rachaelp
    rachaelp over 8 years ago in reply to DAB +2 suggested
    DAB is right, the USB on the Arduino is serial over USB, i.e. it just shows up as a serial port on the PC and you'll probably be maxed out at 115200 baud (I may be wrong here but you should look into it…
  • ripper121
    0 ripper121 over 7 years ago in reply to noblemaster

    Did you get it running?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<