Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Issue to achieve connection with internet in SIM900A
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 0 replies
  • Subscribers 414 subscribers
  • Views 531 views
  • Users 0 members are here
  • arduino uno
  • gsm/gprs
  • gsm
  • atmega328
  • atmega328p-pu
  • arduino
Related

Issue to achieve connection with internet in SIM900A

bhavikbhansali
bhavikbhansali over 9 years ago

Hello all,

 

As I am working on one of the project where we use gsm module which is SIM900A and pushes sensor data into the server through GET POST method. but the this is we are not able to achieve connection with the internet through SIM900A module. Can anybody please help me to solve this to complete the entire project. As the only remain the part in the project is that only. As the problem, we are running a demo code where we try to run the require AT command and still we are not able to achieve this.

 

Arduino code for the same is as below.

 

 

#include <SoftwareSerial.h>

#include <String.h>

 

 

String pid="20170101";

String timestamp="2017-05-05 11:10:20";

SoftwareSerial mySerial(6,5);//rx, tx

 

void setup()

{

  mySerial.begin(115200);               // the GPRS baud rate  

  Serial.begin(115200);    // the GPRS baud rate

 

 

  Serial.println("start"); //to check that program starts or not

  delay(500);

 

 

  mySerial.println("AT+CSQ");

  delay(500);

  ShowSerialData();

 

 

  mySerial.println("AT+CGATT?");

  delay(500);

  ShowSerialData();

 

  mySerial.println("AT+CGATT=1");

  delay(500);

  ShowSerialData();

 

  mySerial.println("AT+SAPBR=3,1,\"CONTYPE\",\"GPRS\"");//setting the SAPBR, the connection type is using gprs

  delay(2000);

  ShowSerialData();

 

  mySerial.println("AT+SAPBR=3,1,\"APN\",\"www\"");//setting the APN, the second need you fill in your local apn server

  delay(2000);

  ShowSerialData();

 

  mySerial.println("AT+SAPBR=2,1");//setting the SAPBR, for detail you can refer to the AT command mamual

  delay(1000);

  ShowSerialData();

 

  mySerial.println("AT+HTTPINIT");

  delay(1000);

  ShowSerialData();

 

  mySerial.println("AT+SAPBR=1,1");//setting the SAPBR, for detail you can refer to the AT command mamual

  delay(1000);

   ShowSerialData();

}

 

void loop()

{ 

String web = "AT+HTTPPARA=\"URL\",\"http://iepmcs.tk/add3.php?ts=" + timestamp +"&pid=" + pid + "&dt=1&at=0&nt=0\""; //timestamp is from rtc ds1307 (code for that is not attach here).

  

mySerial.println(web);

delay(2500);

ShowSerialData();

 

  mySerial.println("AT+HTTPPARA=\"CID\",1");

  delay(500);

  ShowSerialData();

 

  mySerial.println("AT+HTTPACTION=0");

  delay(500);

  ShowSerialData();

 

 

 

delay(5000); //wait for 5 second

}

 

 

 

 

void ShowSerialData()

{

  while(mySerial.available()!=0)

    Serial.write(mySerial.read());

}